STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A bug on pwm complementary output of cubemx32

Posted on June 25, 2017 at 13:07When i want to produce a pwm complementary output ,the chip is stm32f103c8, only main connel have output and auxiliary have no output . I track program to file stm32f1xx_hal_tim.c on funtion : TIM_OC1_SetConfig and fi...

About stm32L stop mode uart

Posted on November 26, 2017 at 13:58hi everyone~Before  enter stop mode ,I called HAL_UART_DeInit(&huart3) an  after it was  wake up from stop mode(wake up by rtc), I called HAL_UART_Init(&huart3),but after wake up uart3 can't work. What should I do...

guo sir by Associate II
  • 1086 Views
  • 1 replies
  • 0 kudos

Nucleo L496ZG-P USB VCP problem

Posted on November 26, 2017 at 17:00Hey Guys,I am trying to sample some ADC and transfer over USB Virtual com port.I managed to get the ADC working but I am facing some difficulties in getting the board to work in VCP mode as the processor gets a sh...

Resolved! STM32CUBEMX FATFS Broken?

Posted on November 21, 2017 at 19:38The original post was too long to process during our migration. Please click on the attachment to read the original post.

con3 by Senior
  • 3954 Views
  • 7 replies
  • 0 kudos

What is FB_Address in BSP_LCD_LayerDefaultInit ?

Posted on November 25, 2017 at 22:05Hi, I am working in stm32f746 discovery board. I want to drive the Lcd. At initialize step, I have to use the BSP_LCD_LayerDefaultInit(uint16_t layerIndex, uint32_t FB_Address).I dont know what  is FB_Address? Can...

How can i use EXTI at SPL?!!

Posted on November 25, 2017 at 15:59hi.i want to write code for EXTI in IAR with SPL library,but i dont know what do i do with spl. i realy need steps of the configration of EXTI setting.who can say  the steps of EXTI to me??do i need configration i...

Failture to start motor with stm32f0 and mc33926

Posted on November 25, 2017 at 12:54Hello,I have problem to start motor with sm32f0 and single motor driver mc33926. I was in pololu forum and they sad that everything connection is ok, but still dont work. I have joystick to control speed motor. Ad...

Failure to start main on STM32F7

Posted on November 21, 2017 at 17:11I am having an issue where STM32F7 fails to start on reset. Here is a section of a startup code which fails:IMPORT SystemInit IMPORT __mainLDR R0, =SystemInit BLX R0 LDR R0, =__initial_sp ; restore original stack ...

stm mass storage usb does not recognize.

Posted on November 25, 2017 at 03:54Hi mass storage is being implemented.Nucleo-F207G is being tested.en.stm32cubef2 \ STM32Cube_FW_F2_V1.7.0 \ Projects \ STM32F207ZG-Nucleo \ Applications \ FatFs \ FatFs_USBDiskThe sample is usb-detectable without ...

0690X00000608wWQAQ.png 0690X00000608suQAA.png 0690X00000608wlQAA.png 0690X00000608wUQAQ.png

How to create SMBus slave?

Posted on November 24, 2017 at 20:52I was using I2C connection between two STM32F030, but decided to try SMBus, because of I2C issues with analog filter, when lines stay high/low. I'm trying to send 1 byte and have issues with slave: master sends ad...

rokko by Associate II
  • 659 Views
  • 0 replies
  • 0 kudos