cancel
Showing results for 
Search instead for 
Did you mean: 

Chaining 16 bit timers to a 32 bit timer. Am I understanding it?

john doe
Lead
Posted on August 09, 2017 at 04:18

Might as well learn something as long as the cubemx app isnt getting it right

I get stumped by the terminology sometimes because it tends to vary in the documentation.

In order to chain together two 16-bit timers into one 32 bit timer, I need to:

set up the first timer as oc output one pulse mode

do I want the slave in reset mode or gated mode?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Tomas DRESLER
Senior II
Posted on August 09, 2017 at 10:39

First timer free running, with master output on update event (i.e. reset of the counter)

Second timer as slave External clock mode with proper ITRx input