cancel
Showing results for 
Search instead for 
Did you mean: 

Issue SPI transfer using HAL_SPI_Transmit_DMA

Posted on August 09, 2017 at 19:41

Hi 

First I will give info about my project.

I am generating PWM using timer, then SPI using Full Duplex slave mode and a GPIO pin. 

PWM is connected to SPI sclk and GPIO is connected to NSS.

I am transferring data from 1 to 550 and 1100 to 1650. Now the problem is the first block of data i.e 1 to 550 going well. when I restart the SPI transfer I see some 2 bytes of junk data that is transferring through SPI. Below is the code and waveform.

Please suggest me and let me know where I am going wrong.

MX_GPIO_Init();

MX_DMA_Init();

MX_SPI1_Init();

MX_TIM3_Init();

/* USER CODE BEGIN 2 */

int j = 1;

for (uint16_t i = 0; i < 1100; i = i+2)

{

testDataToSend[i] = j;

testDataToSend[i+1] = j >> 8;

j++;

}

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);

HAL_SPI_Transmit_DMA(&hspi1, testDataToSend, 1100);

HAL_TIM_PWM_Start(&htim3, TIM_CHANNEL_4);

HAL_Delay(1);

HAL_TIM_Base_Start_IT(&htim3);

while(flag != 1){

}

flag = 0;

for (uint16_t i = 0; i < 75; i++);

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);

HAL_SPI_DMAStop(&hspi1);

HAL_SPI_Abort(&hspi1);

*testDataToSend = NULL;

j = 1100;

for (uint16_t i = 0; i < 1100; i = i+2)

{

testDataToSend_1[i] = j;

testDataToSend_1[i+1] = j >> 8;

j++;

}

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);

HAL_SPI_Transmit_DMA(&hspi1, testDataToSend_1, 1100);

HAL_TIM_Base_Start_IT(&htim3);

while(flag != 1){

}

flag = 0;

for (uint16_t i = 0; i < 35; i++);

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_SET);

*testDataToSend_1 = NULL;

/* USER CODE END 2 */

/* Infinite loop */

/* USER CODE BEGIN WHILE */

while (1)

{

}

/* USER CODE END WHILE */

void DMA1_Channel3_IRQHandler(void)

{

/* USER CODE BEGIN DMA1_Channel3_IRQn 0 */

flag = 1;

/* USER CODE END DMA1_Channel3_IRQn 0 */

HAL_DMA_IRQHandler(&hdma_spi1_tx);

/* USER CODE BEGIN DMA1_Channel3_IRQn 1 */

/* USER CODE END DMA1_Channel3_IRQn 1 */

}

void TIM3_IRQHandler(void)

{

/* USER CODE BEGIN TIM3_IRQn 0 */

HAL_GPIO_WritePin(GPIOA, GPIO_PIN_0, GPIO_PIN_RESET);

HAL_TIM_Base_Stop_IT(&htim3);

/* USER CODE END TIM3_IRQn 0 */

HAL_TIM_IRQHandler(&htim3);

/* USER CODE BEGIN TIM3_IRQn 1 */

/* USER CODE END TIM3_IRQn 1 */

}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0