STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reset source and backup SRAM in STM32F7

Posted on November 30, 2017 at 12:51Hi,I am developing a prototype board which does a set of programmed task and goes to standby mode. It has both clock interrupt and pin wake up interrupt to wake the controller up from the standby mode. I am facing...

Resolved! What is address offset?

Posted on December 01, 2017 at 11:17I am Japanese. Because there is little information on Japanese STM 32, please let me ask a simple question here.What is address offset? According to RM 0364 Reference manual ''STM 32 F 334 x x advanced ARM®-based ...

0690X00000608sQQAQ.png 0690X00000608z3QAA.png 0690X00000608wmQAA.png
Ken Inoue by Associate III
  • 3671 Views
  • 2 replies
  • 0 kudos

Program code different location

Posted on December 01, 2017 at 12:08Hi all,It's possible to use the sector 0 to store the user variable and the other sector 1..31 for the program code?I've tried to set the STM32f072 but remains stuck.Thanks.

Bugs in stm32f10x LL library

Posted on August 21, 2017 at 14:16I tried to use LL library for stm32f10x without CubeMX (  * @version V1.1.1  * @date: 12-May-2017) and almost immediately found some problems:1) You can't actually download LL library without CubeMX, even if you don...

amomum by Associate III
  • 3069 Views
  • 5 replies
  • 0 kudos

CubeMX error code generation

Posted on November 07, 2016 at 12:19When regenerating code (previously correctly generated several times) CubeMX displays an error window and deletes an initialization assembler source file which prevents the Eclipse/System Workbench project to buil...

X-NUCLEO-IHM02A1 w/STM32F302R8 Problems

Posted on November 30, 2017 at 23:43I am using a X-NUCLEO-IHM02A1 dual stepper motor driver evaluation board paired with a NUCLEO STM32F302R8 board. My IDE is the System Work Bench for STM32. The motor driver comes with a software package for contai...

Resolved! STM32F746 Discovery Board External SDRAM Address crash

Posted on November 30, 2017 at 17:28Hi, I'm new here.I've started a project using the STM32F746 Discovery board and I've been messing around with the external SDRAM.I copied the initialisation code from the FMC example, and used STM32CubeMX for the ...