STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Idiots guide required or is it hitch hikers

Posted on January 16, 2018 at 18:07I have got connected a nucleo-f401 with idw01m1.I have tera-term  for terminal things and Firefox as brouser.I have got the server socket compiled and loaded in system work benchAfter some time trying to load dynam...

STM32 gateway LoRa

Posted on January 16, 2018 at 14:21Hello, i want to use 2 STM32 discovery kit, One for the client LoRa and One for create a gateway LoRa.does it already exist a script that works as gateway lora that could works in the STM32 discovery kit? or other ...

Synchronizing SPDIFRX and SAI clocks

Posted on August 29, 2017 at 15:09Hi everyone, For the last week I've been trying to capture a SPDIF stream (at 48000 Hz) through the SPDIFRX peripheral with the STM32F745 MCU and redirect it through a SAI output (connected to an external DAC).The m...

Resolved! STM32F723e-disco HS USB examples - Cube issues

Posted on January 11, 2018 at 18:31I am currently trying to generate a new project for Keil as a HS Custom HID device (eventually it will be composite with another class) and have been encountering enumeration issues.  The code builds, loads, and ru...

STM32Cube4.23.0

Posted on January 15, 2018 at 21:17 Installed STM32Cube4. The icon does not show this is on the desktop (picture attached). When I click on the 'icon' I receive the attached error message: 'The registry refers to a nonexistent Java Runtime Environm...

Optimising for mono audio

Posted on January 15, 2018 at 15:06Hi, I'm prototyping something that processes digital mono audio from a mems mic, transferring the data over i2s into an stm32f373. The only issue I have is that the DMA transfer is designed for stereo so twice as m...

Resolved! mx configuration report

Posted on May 13, 2017 at 09:48A minor bug in STM32CubeMX 4.21.0 (Win7, Adobe Reader 2017):pin names don't fit in generated report PDF when 'locating stake' for user label is used. See attached screenshot

['F446 documentation] SAI clock generator

Posted on January 02, 2018 at 23:49The SAI clock generator subchapter and related comments throughout the SAI chapter are confusing. A complete rewrite would be beneficial, but I doubt anybody is willing to do that. So let me give a couple of simple...

0690X00000609KJQAY.png

STM32F1Cube drivers bug

Posted on January 16, 2018 at 12:25Dear,I am currently using the STM32F1Cube drivers on a STM32F107VC MCU (STM3210C-EVAL board) and I discovered a bug in CAN drivers.The problem is in the 'stm32f1xx_hal_can.h file on line 379.#define CAN_FLAG_TXOK2 ...

Resolved! How to add arm_cfft_q31

Posted on May 08, 2017 at 00:27I have a CubeMX generated project and need to made a FFT in Q31 format on a STM32F103RB nucleo board.I have add this includes#include <math.h>#include 'arm_math.h'#include 'arm_const_structs.h'and add a defin ition for...

leonardo by Associate III
  • 2541 Views
  • 5 replies
  • 1 kudos