STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO state at power down

Posted on February 03, 2018 at 23:40Hello there,According to the datasheet, the GPIO ports circuit diagram looks like this in STM323L4x2:From this diagram I understand that at powerdown (VCC = VSS = 0 V) the I/O pin state is high impedance. But is t...

0690X00000609awQAA.png

STM32F302 change ADC clocksource

Posted on January 12, 2018 at 09:39Hey,in my current ADC code I use the PLL as clock source (72MHz). That causes a problem in the powersave mode, where the PLL is disabled and the clock source of the mcu core is just HSE (12 MHz).Now I want to use t...

Clock configuration tool for STM32F429?

Posted on February 02, 2018 at 12:30I'm looking for a Clock configuration tool for STM32F429. Does one exist?Or can I use the Clock configuration tool for STM32F40x/41x microcontrollers (AN3988)?#stm32-f4

sima2 by Associate III
  • 1673 Views
  • 5 replies
  • 0 kudos

Watch dog in sleep mode

Posted on February 05, 2018 at 15:48Dear,I want to use the watchdog for STM32L0. But do not how to disable the watchdog before going to the LowPower modes (sleep mode). Because if I go to the sleep mode, the watchdog reset my device and wakeup it fr...

JAN R by Associate III
  • 830 Views
  • 0 replies
  • 0 kudos

CubeMX and SysTick

Posted on February 02, 2018 at 16:09Why does CubeMX generate the following lines in SystemClock_Config if the HAL timer is set to anything other than SysTick?HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);/**Configure the Systick */HAL_SYSTICK_CLKS...

adrian by Associate III
  • 6888 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.