STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F746 Startup-Problem with DCache - AN4667

Posted on December 16, 2016 at 11:08Hello,I have problems with a STM32F746 and DCache. Without DCache my software runs perfectly. If I enable the DCache (first invalidate it and the Enable), then I can't start the board.I have check my source code, ...

USB Fifo not empty

Posted on February 06, 2018 at 10:10Hi.I am doing a basic USB device using STM32F407 and the usb Rx and Tx Fifo's look strange. For example data in at address 0x50001000: 00CC0080 01000680 00400000 00C80000. Then is followed by the following ataddre...

ADCx in multichannel with DMA and LL library

Posted on February 05, 2018 at 23:56Hello,I use a STM32F407 on a custom board. The application is in Motor Control. I have to read the next channels:ADC1: Channel 0 and 2ADC2: Channel 6 and 14ADC3: Channel 10 and Channel 11 and Channel 12 and Channe...

HOW TO SET THE BXCAN R1 AND R0 ?

Posted on February 02, 2018 at 18:32Hello, I run the CAN loopback example project by NUCLEO-F446ZE. And find a problem, may I to set the r1 and r0 ? I read the RM0390, no message about it. Could you please let me know How to set the r1 & r0 bits?

Update firmware stm32f103 via SWD

Posted on February 05, 2018 at 10:48Hi! How to update firmware stm32f103 via SWD interface from ESP8266?  I need program manual, application/technical note, or description of SWD interface. Maybe someone did this? #esp8266 #swd #stm32f103 #update-fi...

Sam Sam by Associate
  • 3796 Views
  • 7 replies
  • 0 kudos

STM32L4 DAC for Actuation - 16 Channels

Posted on January 30, 2018 at 17:51 Dear All, I am using STM32L476 to generate actuating signals (50k Sine wave, ±6 V) for 16 piezoelectric actuators. I realize there are just two DAC channels for this MCU. I would like to know what kind of exter...

0690X00000604KTQAY.jpg

How to setup ADC DMA to synch with timer? STM32F4

Posted on March 10, 2017 at 22:43I'm trying to setup 3 ADCs to read on a timer tick. On the STM32cube the timer can be set to 'Output Compare' to a single channel. And the ADC's can be set to external trigger conversion on a 'Timer Capture Compare #...

NOR Write problem (hanging in busy state)

Posted on February 05, 2018 at 19:47We're using STMCube to integrate two types of NOR Flash : MICRON and CYPRESS.We are using the HAL_NOR_ProgramBuffer() function, memory data with = 16 bits.Some tests showed that we could not write over the first o...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.