STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F071V8 ADC ADC_IN17 (VREFINT) measurement errors

Posted on February 14, 2018 at 14:33Hi all,We are using a STM32F071V8 MCU in our project. I am polling the ADC to read the data and have followed the following procedure to initialize the ADC:1. enable clock to respective GPIOs2. Initialize GPIO pin...

Has no detected problem for Blue NRG GUI in STM32F401RE

Posted on February 07, 2018 at 21:14HiI want to evaluate BlueNRG using the BlueNRG GUI. My setup is as follows: NUCLEO-F401RE with X-NUCLEO-IDB05A1 installed. BlueNRG GUI software version V2.2.1 (latest) X-CUBE-BLE1 Cube Expansion packageI've follow...

Activate DFU using HAL driver on STM32F072

Posted on February 16, 2018 at 12:12Hi all,I am trying to set up my STM32F072 device so that I can connect it to my computer via USB and upgrade the firmware using DfuSe software. I did all the wiring to do so but my problem is that I want to activa...

QuadSPI data read as classic SPI

Posted on February 16, 2018 at 10:38Hi all,I am trying to use the QuadSPI of STM32H743 as a classic SPI but using four lines. The point is that quadspi uses several phases  (instrucction, direction, dummy, anternative, data) and I would like to skip...

Bug report in cube MX code generation

Posted on February 16, 2018 at 09:57Hello,I use the cubemx v4.24.0 in AC6' workbench (windows version) for generating LL ADC code, and the channel selection code seems to be wrong, because it overwrites CHSELR for each selected channel, which ends w...