cancel
Showing results for 
Search instead for 
Did you mean: 

Why are cubemx/mcu/IP/GPIO-STM32F10?_gpio_v1_0_Modes.xml not complete?

Uwe Bonnes
Chief
Posted on October 09, 2017 at 11:42

Hello,

for all families beside F1, the cubemx/mcu/IP/GPIO-STM32Xxxx_gpio_v1_0_Modes.xml give a complete list of the available device functions on a pin. For F1 files, only functions available on a pin that may get remapped are listed.

E.g. for F107 pin  PA0, the available function 'ETH_CRS' is only listed in cubemx/mcu/STM32F107XXXx.xml, while mcu/IP/GPIO-STM32F107_gpio_v1_0_Modes.xml does not list it.

Having all information  (pin name, pin function, remap value (no remap., 0..4) comes handy when generating support files from the XML headers.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0