STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTC register write strangeness, F429-446

Posted on February 17, 2018 at 02:53/******************************* Unlock and set clock sources **********************/PWR->CR = (1<<8); //Disable Backup Domain write protectionRCC->BDCR |= RCC_BDCR_RTCEN;    //RTC clock enabledRCC->BDCR |= RCC_BD...

CubeMX 4.23.0 bugs NUCLEO-H743ZI

Posted on October 25, 2017 at 18:27Hi guys.1.)I already mentioned a bug in the previous CubeMX release.Enabling Ethernet CubeMX reservesPB12 for ETH_TXD0andPB11 for ETH_TX_ENand writes the wrong settings in ethernetif.cBut it must be:PG13 for ETH_TX...

Resolved! jtag connectivity to custom board based out of stm32f7

Posted on February 15, 2018 at 20:30Hello we have a customized having stm32f769bitb MCU. i am able to connect JTAG in hotplug mode but when im trying normal and other mode i m getting error as 'cant reset the core'. also i tried connect under reset ...

Resolved! Which register selects the clock input to a STM32F303K8

Posted on February 16, 2018 at 19:22The clock diagram in RM0316 for the 32F303K8 indicates a clock selection mux off the APBx prescalers. I've searched the registers and cannot find the register used to select one of 4 clock inputs. The 4 possible i...

STM32F303RE ADC2+DMA2 Don't working

Posted on February 12, 2018 at 16:09HiI am trying to develop a project via the STM32F303RE Nucle Board. In the project, I need to read analog data from channel 0 (PA4) on the ADC2 hardware.  For this I made an init code.void ADC_DMA_Configuration(vo...

0690X00000604NIQAY.jpg

FMC concurrent usages and priority (SDRAM and NOR/PSRAM)

Posted on February 16, 2018 at 17:24High-Level question Detailed descriptionI have two parallel usages of the FMC on an STM32F4 processor: - One that writes to SDRAM with DMA2 Stream 1 - One that reads from an external ADC (FMC NOR Flash/PSRAM contr...

yves by Associate
  • 1084 Views
  • 0 replies
  • 0 kudos

Is the USB library threadsafe?

Posted on February 16, 2018 at 17:10I am developing on the STM32F0 using the USB library and encounter problems when my main routine starts to send data early after the device received the SetConfiguration request.So far I could narrow it down to th...