STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo64 Power Measurement

Posted on February 26, 2018 at 17:34I'm measuring the current on JP6 (IDD) and I see 4mA at the lowest when running the Power_Management sample or even holding the MCU in reset. I am powering the board via the USB connector. Is this incorrect?I've t...

Konami by Senior II
  • 3642 Views
  • 14 replies
  • 0 kudos

FatFs f_open() fails after upgrading to STM32F4 FW pkg 1.17

Posted on November 03, 2017 at 19:53 I have two versions of my project exported from the CubeMX, one for the MDK-ARM and the other for the gcc-based Eclipse IDE (AC6). Both projects built with STM32F4 firmware package 1.1. After upgrading the fir...

Zaher by Senior II
  • 12435 Views
  • 29 replies
  • 0 kudos

STM32F072C8T6 USB-C : X-CUBE-USB-PD

Posted on February 26, 2018 at 17:37HelloI would like to use an STM32F072C8 instead of STM32F072RB with ST example : MB1303ConsumerRTOS.To ease the task, I would like to know, if it was possible to have the Cube configuration of the design. The STM3...

Configuring CAN - error with CubeMX 4.24 STM32F4 1.19.0 ?

Posted on February 26, 2018 at 17:15I try to configure a CAN peripheral in the same kind as before. I want to use the new CAN driver functions.As soon as I’am setting the clock to HSE and 168 MHz no change in CAN is possible. Setting Clock to HSI se...

fe3 by Associate III
  • 711 Views
  • 0 replies
  • 0 kudos

Bugs in F7 Examples - STM32Cube_FW_F7_V1.9.0

Posted on February 21, 2018 at 18:46Wrong interrupt name, doesn't match macro, missing DMA_Tx handlerSTM32Cube_FW_F7_V1.9.0\Projects\STM32F769I-Discovery\Applications\Display\LCD_PicturesFromSDCard\Src\stm32f7xx_it.c (and .h).../** * @brief Handles ...

LoRa beginner

Posted on February 25, 2018 at 18:11Hi. I need to start to use the sx1276 for LoRa implementation.I looked that there is a demoboard that support mbed but I think it is not good for me because I can't use mbed libraries and I need to implement LoRa ...

Stm32f103 CAN

Posted on February 26, 2018 at 14:37Hi friends,I am using first the CAN protocol and what I didnt understand is STM32F104 contain just master CAN ,is it possible stm32f103 to stm32f103 CAN protocol?

Zek_De by Senior
  • 692 Views
  • 0 replies
  • 0 kudos