STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 SDADC phase delay ?

Posted on February 28, 2018 at 09:14Hello everybodyDoes anyone have experience with the SDADC of the STM32F373?I have the following question:Theoretically, my phase delay would have to be at aSampling frequency of 50kHz and output to the 12bit DAC b...

roger by Associate II
  • 2512 Views
  • 6 replies
  • 0 kudos

STM32L4 PWM Phase Delay

Posted on February 19, 2018 at 19:02 Hello: Using the Nucleo STM32L476RG demo board. On an STM32F4xx, using CMSIS, I am able to create 2 PWM pulses that have the same period. However, the 2nd pulse is delayed by: TIM4->CNT = TIM3->CNT + (timerP...

what's address of VREFINT_CAL in STM32F103?

Posted on March 01, 2018 at 02:15I can not find it in datasheet in 'Embedded reference voltage' section.I also try use STM32F0/STM32F405/STM32L486 address. all these address are wrong.#vrefint_cal #stm32f1 #internal-reference-voltage-calibration-val...

wenjin by Associate II
  • 2469 Views
  • 3 replies
  • 0 kudos

An interrupt question of STM32F103RCTx

Posted on March 01, 2018 at 01:52Hello predecessors,I would like to ask a question about external interrupt.I tried to use STM32F103RCTx to develop a Galileo Signal Generator.Development environment is STM32CubeMX + Keil uVision5.TIM2 produces 6M Su...

0690X00000604FHQAY.jpg 0690X00000604R5QAI.jpg 0690X00000604QvQAI.jpg

Video streaming on STM32F429 Disc board

Posted on March 01, 2018 at 02:45Hi All,Board : STM32F429I-DISC1      I am trying to video stream using a camera onto the LCD of this DISC1 board. I read that the LCD used in this board has two layers layer0 and layer1. So is it possible to do video...

STM32CubeMX for STM32L432KCU6

Posted on February 22, 2018 at 15:24Hello,Have a STM32L432 Nucleo 32 board. I am using the CubeMX to initialise some code and I see in Workbech that within drivers/CMSIS  there are much more files that others STM32 projects.The point is that there t...

Infinite_Loop during UART operation

Posted on February 28, 2018 at 11:35 Hi, I am using STM32F446RETxNucleo board formy application. It was working fine till I added a new operations including asynchronous data exchange on UART5. Now, sometimes during data exchange on the seri...

STM32L0 ADC clock source and CubeMX

Posted on January 18, 2018 at 17:49Hi everyone!  I'm using an L071CBTx and I'm trying to figure out how to change the ADCs clock source using CubeMX.  According to the reference manual, 'the ADC can be derived either from the APB clock or the HSI16 ...

Jim Kaz by Associate II
  • 2483 Views
  • 3 replies
  • 0 kudos

Reliably detecting power-off/on with stm32l432

Posted on February 28, 2018 at 16:24The stm32l432 lacks the PORRSTF flag that other stm32 processors have, so I don't see a way to reliably detect a power-off/on event.  I tried parking a bit in the backup registers, but it doesn't appear that this ...

What happens when I turn off a peripheral clock ?

Posted on February 28, 2018 at 09:08Hi, I'm designing a low power application using a L452RE. In order to keep the power consumption to the minimum I turn ON and OFF the peripheral clocks only when I need to use the peripheral. My question is what h...

Kraal by Lead
  • 3181 Views
  • 6 replies
  • 0 kudos