User Activity

Posted on October 10, 2017 at 17:24I'm looking to use the FMC in Synchronous PSRAM 16-bit mode, and need to run CLKDIV of 3 (or 4).  The reference manual (RM0410) waveforms seem to show only a setting of CLKDIV=2.  In figure 50/51, CLK is shown togg...
Posted on December 12, 2016 at 15:00I'm currently using the STM32F051R8T6, 64 pin LQFP.  Is the STM32F091RCT6 in the same package fully pin-compatible?Thanks,Paul♯♯♯#stm32f091 #compatible #stm32f051
Posted on January 25, 2013 at 21:47Hi, Just opened a STM3240G-EVAL kit.  I'm trying to get the STM32F2-F4 Demonstration Builder to run, without much success.  If I download the prebuilt binary ''STM324xG_EVAL_Demonstration_Builder_V1.3.0.hex'', it r...