STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX SD_status with FreeRTOS not reentrant

Posted on March 10, 2018 at 08:38 The follow code snippet is generated in sd_diskio.c by CubeMX (4.0) when using FreeRTOS (STM32Cube_FW_F7_V1.9.0): /** * @brief Gets Disk Status * @param lun : not used * @retval DSTATUS: Operation status *...

Where are any B-L475E-IOT01A CUBEMX examples?

Posted on March 09, 2018 at 16:12Where are any STM32Cube example projects for the B-L475E-IOT01A board?    I can find the generated projects for example BLE/HeartRate and P2P_LedButton.   But how were these generated?  Isn't the whole point of using...

STM32F031C6T forward compatible to F051, F071 and F091

Posted on March 09, 2018 at 16:21We are working on a motor controller and started with a evaluation board that uses the STM32F031. Unfortunately we have utilized over 80% of the flash and 90% of the RAM, so going forward with the STM32F031 is a bit ...

gerald23 by Associate II
  • 1442 Views
  • 2 replies
  • 0 kudos

Jitter less than 20ns with STM32L476

Posted on March 08, 2018 at 16:28Hi, I've a problem with the jitter of my program on STM32L476.First of all, I'm introduced you my project.A signal TLL with a frequency of 1KHz to 50 KHz must be multiplied by a sinusoide or square analogique signal ...

Why doesnt the Tc flag in usart clear?

Posted on March 07, 2018 at 22:25HiI use stm32f407 to communicat with rs485.I use DMA to transmit data. For controllig dirction pin, I check the USART_FLAG_TC. Whet it is set, I will push Dirction pin low and clear the USART_FLAG_TC by writing with ...

Resolved! Why people got their answer but not mark correct

Posted on March 08, 2018 at 04:58First of all, Thanks for the help from community. I hope I could be more helpful, more healthy and strong.I saw many questions were answered but the author don't mark correct. Some of the thread were many years ago.I...

ETHERNET SEND AND RECEİVE SAME TİME

Posted on March 09, 2018 at 16:36We are trying to establish and send and receive Project through an ethernet connection .we use Nucleo f429ZI, We have our nucleo with static  ip 10.1.1.2 mask  255.255.255.0 gateway 10.1.1.1 using cubemx ,PHY 0,pc is...

Resolved! STM32 uVision - missing pack

Posted on March 08, 2018 at 15:22I attended the STM8-32 hands on day in Cambridge in Feburary 2018.I have been repeating or doing the exercises that we did on the day but I have been unable to program the target STM32F072RB nucleo board in three of ...