cancel
Showing results for 
Search instead for 
Did you mean: 

Why does CubeMX only allow SD High Speed in 32L4Rxx and 32L4Sxx?

pauljohnston
Associate II
Posted on November 17, 2017 at 01:27

I generated the code for a STM32L496 that hopes to use the SDIO with an external SD card. To meet my data throughput, I will need the 4 bit bus and the high speed mode which the L496 appears to have. However, the generated code has restricted these two features to only STM32L4Rxxx and STM32L4Sxxx versions of the chips (using &sharpif defined...).

What am I missing?

#sd-high-speed #sd-4-bit-data ##if-defined(stm32l4r5xx)
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0