STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FATFS Unlink driver

Posted on March 12, 2018 at 16:54 Hello, I have problem when I use FATFS with my STM32F2. My code come from example STM32-Tools\STM32_FW_libraries\HAL_CUBEMX_libs\STM32Cube_FW_F2_V1.6.0\Projects\STM32F207ZG-Nucleo\Applications\FatFs\FatFs_USBDi...

Eclipse+Gcc project tree question

Posted on March 12, 2018 at 16:40Hi there,I've set my STM32 toochain with Eclipse Oxygen + GCC + GDB + OpenOCD and I play with a STM32F769 discovery board. I could compile and debug the blinky project properly. Now I'd like to start a new project. I...

Problem in file system update using UART in SPWF01S

Posted on March 12, 2018 at 15:11In SPWF01S wifi module, could perform File system update using AT+S.HTTPDFSUPDATE over the air with the help of Apache web server successfully (from Lab6 of Wi-Fi Training - Hands On  manual). But the same is giving ...

How to single stepping debug STM32F091

Posted on March 09, 2018 at 14:33 I have several STM32 CubeMX / HAL projects and I use EmBitz as IDE. All porjects working fine, including compilation and debugging. There are projects with STM32F103, STM32F205, STM32F207,STM32F405, STM32F429, STM3...

use dfsdm with parallel input

Posted on March 11, 2018 at 16:38Hi,I have get pdm data and want to use dfsdm to convert to PCM.The test code is like below:HAL_DFSDM_FilterRegularStart(&hdfsdm1_filter0); uint16_t *pdm_data=... for (int i=0;i<pdm_size;i++) { hdfsdm1_channel1.Instan...

hgyxbll by Associate II
  • 1729 Views
  • 2 replies
  • 0 kudos

issue with DCache on STM32F746ZG

Posted on March 11, 2018 at 16:54Hello, i'm having issue on STM32F746ZG, connected with ETH PHY through RGMII, and i'm having also enabled USB HS using ULPI, when i not enable DCache at start everything works perfectly ...but when i enable SCB_Enabl...

STM32F042 IAP Problem

Posted on March 12, 2018 at 12:46Hello,       I want to write a 'User Application' for the USART bootloader (AN4657) provided by ST.        I modifed the CubeMX generated code like below;       My code is not working properly. When I debug my code, ...

Unable to retrieve the data from external flash

Posted on March 12, 2018 at 12:46I am using STM32L100 to interface the External Flash through SPI but unable to retrieve the data from flash, using SPI_I2S_SendData library function to send data and SPI_I2S_ReceiveData library  function to retrieve ...