STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F04xx USART Idle line detection

Posted on March 09, 2018 at 13:19I have been trying to use the USART idle line detection flag to  detect when an incoming transmission stream has ended. if((USART1->ISR & USART_ISR_RXNE) != RESET) {   if ((1+RX_BUFFER_POS) < RX_BUFFER_SIZE) {       ...

Tom Eaton by Associate II
  • 4001 Views
  • 3 replies
  • 0 kudos

MXCube F302 timer driver will not compile from generation

Posted on March 07, 2018 at 16:13using mxCube 4.24.0Keil 5.25.0.0using timer             :6 prescalar                :64Counter                  :upCounter period      65535autoload preload  : disable Cube produces void MX_TIM6_Init(void){  TIM_Mast...

dcurran2 by Associate II
  • 3596 Views
  • 8 replies
  • 0 kudos

TCP communication problem.

Posted on March 09, 2018 at 11:41Hi,how we can communicate multiple tcp clients to a tcp server simultaneously using  FREERTOS?with regards,SunilCalixto Firmware Team

STM32L073 + sx1272 (downlink rssi)

Posted on March 09, 2018 at 05:13Hello,I'm using LoRa network with sx1272 + stm32L0 (node),and RAK831 (gateway) , also custom network server.i found that uplink rssi printed in gateway is quite good enough(-32dBm), however, downlink rssi printed in ...

Chris Oh by Associate II
  • 1246 Views
  • 2 replies
  • 0 kudos

STM32F411 which display to add?

Posted on March 09, 2018 at 09:38I want to add a display to my stm32F411.I'm relatively new to the STM platform. Can somebody advise me a display and protocol to use which is general in STM world?Similar question about how to add a network connectio...

Cannot install STM32 Cube programmer for MAC

Posted on February 12, 2018 at 15:54Hello, I'm having troubles installing STM32Cube Programmer under MAC - High Sierra, recently formatted.The installation process starts regularly and then freezes forever!Can anyone help me??Regards :)

STM32L432 LSE startup timeout with CSS enabled

Posted on March 09, 2018 at 08:35if Clock security system on LSE is enabled:After a few power on/off/on cycles, Clock security system protection always is triggered.  Only power off for more 5s will reset protection bit.Currently I disabled clock se...

Darius B by Associate II
  • 834 Views
  • 0 replies
  • 0 kudos