STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

wake up from stop mode using I2C on X revision

Posted on March 20, 2018 at 10:46Hi everybody,I'm trying to wake up the MCU STM32L051T6 from stop mode using I2C.i saw that it is a very common problem.i read the errata sheet and it reports tha on X revision the problem is fixed.Now i'm using the r...

STM32F0 WITH RN2485 LORA,RADIO TX RESPONSE ISSUE

Posted on March 17, 2018 at 12:33Hello,I have a customized board for STM32F030R8x microcontroller interfaced with Microchip Lora Module RN2483 over UART.I want to establish P2P connection between Lora module. When i am connecting the modules directl...

Resolved! STM32F1 and TIM3 PWM - LL drivers

Posted on March 19, 2018 at 20:11Hi,Today's F1 v1.6.1 HAL driver pack fixed all issues I had with GPIO so decided to move forward with TIM3 and LL.The goal: use TIM3/PWM to blink the BLUE LED (PC8) - STM32VLDiscovery.CubeMX generated code:/* TIM3 in...

0690X0000060A51QAE.png

I2C Multimaster

Posted on January 12, 2018 at 11:12Hi,We have a 'distributed' system in place where we have a single I2C master (STM32F7) and a number of I2C slaves (STM32F0).  I understand that I2C multimaster is supported, where you have a number of masters speak...

Forced output mode [17.3.7]

Posted on March 19, 2018 at 18:15Hi, I'm currently using an STM32F413 and I would like to use the forced output mode on the TIM1 with 3 PWM already configured. I followed the instructions noted in the reference manual [17.3.7] : - CCxS bit to 00 in ...

0690X00000604UiQAI.jpg 0690X00000604UnQAI.jpg
Jems On by Associate III
  • 2063 Views
  • 2 replies
  • 0 kudos

SD card access through MSC

Posted on November 24, 2017 at 22:21Hello,I am trying to make a MSC USB device to access SD card files.The computer recognizes the mass storage device, but cannot open the folder. After a while, it says the device was unrecognized.My code from usbd_...

Resolved! STM32F1 - LL_GPIO_Init() problem

Posted on March 17, 2018 at 20:45 Hi, A piece of code from STM32CubeMX v4.0 and latest F1 drivers generated for STM32VLDiscovery (the button is pulled-down by external resistor): static void MX_GPIO_Init(void) { LL_GPIO_InitTypeDef GPIO_Ini...

0690X0000060A77QAE.png 0690X0000060A9WQAU.png

Nanosecond delay

Posted on March 18, 2018 at 15:32 EDIT: Not sure where my intro paragraph went on the first time I posted. I have the below code working with inline assembly nops. Now I want to have the code be clock independent. The below code is my attempt ...

joe23 by Associate II
  • 4358 Views
  • 9 replies
  • 0 kudos