STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 PMSM foc sdk 5.0 serial communication

Posted on April 05, 2018 at 04:11I am working with stm32 PMSM foc sdk 5.0. I want to drive the system by the application board and it can send a command to the motor drive board and get a feedback.The application board and motor drive board communic...

HAL_FLASH_OB_Launch(), holding..

Posted on April 05, 2018 at 03:50Hi.I am going to set the RDP-Level 1 programmatically.Here is the test code:Here it stops at the HAL_FLASH_OB_Launch () function.The Reset button does not work in this state.The USB connection will work only if you r...

Jin ho An by Associate II
  • 1038 Views
  • 0 replies
  • 0 kudos

STM32F303VCT6 ADC input imedance

Posted on April 05, 2018 at 02:00What is the ADc input impedance on the  STM32F303VCT6? How to decide of ADC input sampling time? My signal is very low frequency (10 kHz).Please let me know.Channamallesh

''USB On-The-Go Host'' or ''USB Host''?

Posted on April 02, 2018 at 23:30Hi everyone,I'm working on a board based on STM32F4XX. We plan to support USB Host on it for communication(CDC). I found there are 'USB On-The-Go Host' and 'USB Host' libraries. I'm not sure which one to use.First, I...

Pilot B by Associate II
  • 2066 Views
  • 7 replies
  • 0 kudos

Use I2S_CKIN external clock source for SPI?

Posted on April 04, 2018 at 17:08Is it possible to use the I2S_CKIN external clock source for SPI rather than come off the peripheral clock? From the reference manual it appears that this external clock is available as a source only when the SPI is ...

Option to generate C++ project (for SW4STM32)

Posted on December 29, 2016 at 11:21Hello,Currently, there is a possibility to generate C projects for different IDEs including SW4STM32, which uses gcc for compilation. But one can also use C++ code with g++ compiler supporting cool c++11/14 featur...

AES feature in STM32F733ZE

Posted on April 02, 2018 at 08:32I'm going to using AES feature in STM32F733ZE  but the the datasheet doesn't have much information regarding AES .Do you know how much speed of AES in the STM32F733ZE  ? And do we have any any demonstration evaluatio...

Hau Lam by Associate II
  • 3082 Views
  • 7 replies
  • 0 kudos