STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Increase the intensity of white led

Posted on April 04, 2018 at 17:29Hi , I want to drive White Led 7 Segment Display. MCUs power supply is 3.3V (STM32F030C6T6), and white led voltage about 2.8V when the current is 20mA. So, light intensity is too low. Is there any way to increase int...

Resolved! CubeMX : Adding Additional expansions

Posted on April 04, 2018 at 18:17How can I add STs expansion packs. http://www.st.com/en/embedded-software/stm32cube-expansion-packages.html?querycriteria=productId=LN1920 But how can I add them, a timer tool could be useful.There was a thread about...

LMI2 by Lead
  • 973 Views
  • 1 replies
  • 0 kudos

FMC-SDRAM

Posted on April 03, 2018 at 07:49Hello, I will use FMC for SDRAM. I looked examples and tried. But this examples used Bank2, I want to use Bank1. How can I do ?

Timer Interrupt not working on STM32F103C8

Posted on April 04, 2018 at 14:51I am using CubeMX and SW4STM32 to generate timer update interrupt on STM32F103C8. The core is running at 64 MHz, and I have verified that other functions like GPIO, PWM, ADC work perfect.The target is to generate an ...

STM32L452 SystemClock_Config with STM32CubeMX

Posted on April 03, 2018 at 12:27Hi,I have Nuckeo-L452RE with STM32L452RE uC on board.This uC max speed is 80MHz.But after enabling MCO on pin PA8 in STM32CubeMX and generating the code to Atollic, I could see wrong SYSCLK frequencies.The reason of ...

Where are _IRQHandler functions defined?

Posted on March 04, 2017 at 16:13Ok so I am talking about the IRQ handlers for ADC, SPI, I2C USART etc.. I am expecting to see weak definitions of ADC_IRQHandler() function for example somewhere...but my startup_stm32.s file in startup directory doe...

NUCLEO-F767ZI Demo Software

Posted on April 04, 2018 at 16:58Where can I find the source of the demo software which is already loaded on a 'fresh from the box' NUCLEO-F767ZI please. I searched the forum and looked on the ST nucleo web pages already.Thanks - John F.

John F. by Senior
  • 2098 Views
  • 3 replies
  • 0 kudos

Resolved! USART3 voltage level

Posted on April 04, 2018 at 22:31I'm using STM32F207ZG ,What is maximum Voltage level at Tx and Rx pin in USART3? Can I use 5V CP2102  USB to TTL converter with STM32F207ZG?