STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 Triple ADC Conversion Not Supported

Posted on March 16, 2018 at 02:22Hi All,Contrary to what the http://www.st.com/resource/en/application_note/dm00337702.pdf document says about the H7 chip, it does not support Triple ADC Conversion mode. It only supports double conversion mode betwe...

JacobV by Associate II
  • 1226 Views
  • 1 replies
  • 0 kudos

Clk Configuration problem

Posted on April 10, 2018 at 12:43Hi, the problem is not solved, below is the clock configuration, Based on the figure above, I tried to use the different divisions /1, /8.. and the different clk (PPLCK, SYCLK, HSE...)  to obtain the correct frequenc...

0690X0000060AVrQAM.png 0690X0000060AVmQAM.png 0690X0000060AKuQAM.png 0690X0000060AVwQAM.png

[STM32L073RZT6] Read USB pins from GPRS modem

Posted on April 03, 2018 at 13:33Hello everybody,I would like to read the USB_DM and USB_DP pins from a GPRS module (it only works in Device mode) with the STM32L073RZT6 microcontroller which has also USB pins available. However, I realized that it ...

STM32F429 Cortex M4 MPU Crash Freertos

Posted on April 10, 2018 at 10:27Hi,We have been trying to use ARM_CM4F_MPU port in one of our application. Freertos version is 10.0.0.An unprivileged task always Mem Faults when trying to use a kernel API though mpu_wrappers is elevating the privil...

Mit N by Associate
  • 718 Views
  • 0 replies
  • 0 kudos

Fatfs f_close causes idle hook

Posted on April 09, 2018 at 08:38Hello everyone I use stm32f746 discovery board. I implemented emwin,Free rtos and Fatfs for the SDcard(using SDIO interface). In my application after pressing a button, a value(as a string) is saved in the SDcard....

Resolved! Debug stuck in LL_RCC_PLL_IsReady

Posted on April 09, 2018 at 16:58 Hello, I have a Nucleo-L476RG and I am trying to debug using openocd. I am able to reach main() function, but when it calls SystemClock_Config() get stuck in:while(LL_RCC_PLL_IsReady() != 1) The firmware...

Resolved! STM32H743 Nucleo DMA transfer error

Posted on April 07, 2018 at 15:15Hi all,To start with:Board: STM32H743ZI NucleoIDE: Attolic TrueSTUDIO for STM32 9.0.0HAL version: STM32Cube_FW_H7_V1.2.0I'm trying to trigger a DMA transfer on DMA1_Stream7 using TIMER 3 CC3.  I want to trigger a tra...

0690X0000060AH8QAM.png

Resolved! STM32Cube_FW_F4_V1.18.0 + SDIO + FATFS R0.12c doesn't work

Posted on December 02, 2017 at 16:56I tried to use the FAT file system with a SD card and the SDIO protocol, but with the v1.18.00 of stm32Cube for F4 MCU's doesn't work correctly, I discovered the next issues.1.-  Inside of the FATFS configuration ...

my computer show did not recognize stm32 ....

Posted on April 09, 2018 at 18:06Hi, i facing a problem. When i connect stm32 with USB cable to my computer, my computer show did not recognize this devices. Although i already install the  STM32 Virtual COM port driver and follow the instruction.

Tan Wen by Associate
  • 1143 Views
  • 1 replies
  • 0 kudos

f_print vs F_write in FatFs

Posted on April 06, 2018 at 07:04I am working with F746G-Discovery board running the project application FatFs_uSD built in the repository.  The application runs using the code as is which writes the data to the uSD with the f_write function.  There...