STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Weird behaviour of WFI instruction on stm32L031G6

Posted on April 10, 2018 at 16:23Hello,I found that WFI instruction modify R0 register value. This happens at least on SysTick interrupt. Value, if modified, appears to be mostly 0, but sometimes is random.WFI behave weird on stm32L031G6, but works ...

SPI Issues: NSS stays low, clk pol high toggling

Posted on April 12, 2018 at 18:46Using STM32F0 device and having some trouble with NSS hard output returning high after transaction, and also when using idle high clock polarity the preamble idle state is changing.  Sometimes it toggles high before ...

How to enable GPIO 5V tolerance

Posted on April 12, 2018 at 14:37Hai,we are using a STM32F070RBT6 controller for development  i need a clarification regarding I/O'sif we want use FT 5 V tolerant I/O we need add any external component or just enable has high.ThanksRakshith

LCD Suggestion to optimize CPU time.

Posted on April 12, 2018 at 15:52Suggestion to optimize CPU time.Hello,I'm working on STM32L433 device and I use the LCD peripheral embedded. The CPU executes my main loop every 50ms, like the description below. And I refresh the LCD display at each...

thln47 by Associate III
  • 2352 Views
  • 1 replies
  • 0 kudos

I2C config on STM32F446xx

Posted on April 12, 2018 at 09:36I use Nucleo64 STM32F446REI want to configure I2C peripheralIn Reference Manuel RM0390 , �24.6.2 I2C Control register 2 (I2C_CR2), it's specified for Bits 5:0  FREQ[5:0]: Peripheral clock frequency :'the maximum freq...

Break condition for TX Uart in F103

Posted on April 12, 2018 at 14:15Hi all,To start with, I am using Peripheral libs for my UART driver.I am trying to wake up a RN2483 LoRa module from its sleep mode. I have on the manual that I need to produce a break condition followed by am 0x55. ...

P M by Associate III
  • 854 Views
  • 0 replies
  • 0 kudos

STM32F429 Bootloader

Posted on April 12, 2018 at 13:51Hello everyone,I want to do bootloader for stm32f429. for this, what are the differences between JTAG and SWD ? Can I use SWD or not ? 

STM32F401 UART pull up to 5V on RX

Posted on April 10, 2018 at 17:58Hi all,Checking a schematic of an RX485 transceiver connected to STM32F401 UART, I got into this detail that captured my attention:The RX line is directly connected to the RX pin of UART1 of the the MCU and it is pul...

0690X0000060AVDQA2.png