STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sample sfecific ADC channel

Posted on April 12, 2018 at 12:41Hi,I'm trying to work with the ADC of the STM32F072RB which have 1-ADC with 16 channels,what I'm trying to do is to take 1000 samples of ADC_CH1 every X second and take 1000 samples of ADC_CH2 every Y seconds and onc...

Ariel G by Associate II
  • 936 Views
  • 1 replies
  • 0 kudos

Bootloader jump to user code

Posted on April 11, 2018 at 15:22I am able to jump from User code into the built-in bootloader without any issues, I am also able to upload the new .bin file using the UART and ST FLASHER Demonstrator, however when I tick the Jump to user code optio...

STM32F334R8T6 can not read memory

Posted on April 12, 2018 at 10:08I have designed a board with STM32F334R8T6. The STM32 pins are configured as in the attached file (I do not think there is a problem here since I have already used the same configuration without problems). The microc...

NUCLEO-F767ZI CAN bus example

Posted on March 27, 2018 at 12:17Hello, is there a working example for CAN bus on NUCLEO-F767ZI board? I tried to search the STM32F7-Cube and was not successful. Thank you in advance! Vaclav#can-interface #stm32f7

Resolved! Event change state output pin in example TIM_OCToggle

Posted on March 26, 2018 at 12:53Hi, i have implemented the example TIM_OCToggle from stm32f40xx to stm32f103xx, both work fine.I want a event in the moment change state output pin of the channels OC, as occurs in the events:HAL_TIM_PeriodElapsedCal...

Resolved! Migration from STM32F105 board to STM32F411 board

Posted on April 09, 2018 at 08:27Hi every body,Really I need your help in order to see if there are any extra change in the schematic side.Right now I use the same board used for STM32F105 to my new STM32F411.What I did:  - I just change the old mic...

Questions about SystemClock_Config() generated by cubeMX

Posted on April 12, 2018 at 08:23The SystemClock_Config() function is generated by cubeMX in main.c. It configure the different clocks used by the system. The question is that it handles the systick timer count in this way:HAL_SYSTICK_Config(HAL_RCC...

Kefei Yao by Associate III
  • 856 Views
  • 0 replies
  • 0 kudos