STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

To know the Register value to read ADC Converted Data

I am writing the code to read the ADC data from internal temp sensor and ADC.I want to know that what is the register value to read the ADC data from there. I am using STM32H743ZIT6 Micro controller. We are  using ADC3,The ADC is set to 16-bit resolu...

Saranraj by Associate II
  • 1723 Views
  • 10 replies
  • 1 kudos

Resolved! STM32H503 External Interrupt HAL Library Doesn't work

Dear All,Recently I am learning STM32H503CBU6, but I find the external interrupt doesn't work with HAL library. I want to get reference from official example code, I only find external interrupt example code with LL library in official SDK. I think S...

Screenshot 2025-03-15 234431.png Screenshot 2025-03-15 234452.png Screenshot 2025-03-15 234210.png Screenshot 2025-03-15 234233.png
Gerald_W by Associate III
  • 1772 Views
  • 3 replies
  • 2 kudos

Invalid initializer error

Hi, it's my first post here. Im learning to use UART and I'm getting a "invalid initializer" error while debugging this code. Can someone please explain why?

Resolved! SPI + DMA Chip Select Data Synchronization?

Hi everyone,I am currently working with an STM32G071. It receives data over the SPI in slave mode. The data is packet based, each currently has 4 bytes, but that will differ in the future. A single chip select sequence may contain multiple packets, b...

Fabian21 by Associate III
  • 6486 Views
  • 7 replies
  • 0 kudos

Resolved! STM32G0B1CET can't connect under SWD

Hi,I have built a handful  of STM32 designs before and never had a chip fail to connect. I can't seem to get any connection in Cube Programmer at all:VDD,VREF+,VBAT is at 3.3V, VSS is connected to ground.NRST is high at bootI can see current drop fro...

jakobnator_0-1741569762772.png jakobnator_1-1741571188367.png jakobnator_2-1741571236810.png

Uart data register flush out

Hi,I am currently using f446 nucleo board with  some over uart interface.I am able to send the desired frames over Uart to sensor and sensor is properly responding by sending positive acknowledgement to each uart sent frames.And this verified in logi...