2024-05-05 11:18 PM
I'm trying to use the RAMECC monitoring subsystem on an STM32H743 but there's some behaviour I don't understand. I've read the reference manual (RM0433 rev 7) and application note AN5432, as well as some related forum posts here.
If I set an interrupt enable bit in one of the RAMECC_MxCR registers then I get interrupts even if none of the interrupts are enabled in RAMECC_IER.
So it seems like the interrupt enables in RAMECC_MxCR are independent of the per-monitor interrupt enables in RAMECC_IER.
Is this the intended behaviour? It's unclear to me from the reference manual and AN5432.
Solved! Go to Solution.
2024-10-25 2:31 AM - edited 2024-10-25 3:14 AM
Hello @KORourke
yes RAMECC_MxCR are independent from the RAMECC_IER global interrupt bits.
Note: you mention AN5432 above, it should be AN5342 .
I will push some inputs to the AN5342 to clarify this point.
Best regards,
Younes
2024-10-25 2:31 AM - edited 2024-10-25 3:14 AM
Hello @KORourke
yes RAMECC_MxCR are independent from the RAMECC_IER global interrupt bits.
Note: you mention AN5432 above, it should be AN5342 .
I will push some inputs to the AN5342 to clarify this point.
Best regards,
Younes