STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does anyone know the correct USB driver for Win10???

Posted on May 06, 2018 at 02:29Much frustration.  Virtual COM driver works perfectly with CDC on Win10.  Supplied DFUSE drivers apparently are not completely compatible.  Anyone got a clue as to which USB driver and gotten from where will actually w...

How to TIMEOUT within DFU bootloader?

Posted on April 23, 2018 at 18:55My STM32F405 widget uses the DFU bootloader to reflash:  the user holds down several buttons in a super-secret pattern, and my firmware jumps to the bootloader.....  at which time DeFUse software can a) reflash over ...

Goof Ball by Associate III
  • 1555 Views
  • 1 replies
  • 0 kudos

STM32F030CCT crashes when AHB prescaler is 8 or higher

Posted on May 04, 2018 at 20:36When trying to set up RCC as the following using Cube, the microcontroller seems to crash.      RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV8;  I checked that the RCC_SYSCKL_DIV8 macros (and higher options) actuall...

Single bulk memory copy (instead of memcpy)

Posted on May 04, 2018 at 15:24We are using STM32-767ZI and copying a small array into a memory area which is mapped to an external FPGA.Looking for how to make the copy in a single bulk operation.The options are:1. with a loop:        while(i < des...

Resolved! Capacitive touch sensing for STMF103

Posted on January 12, 2018 at 12:46Hello,I am trying to implement a long 1D capacitive touch slide sensor or around 7 or more separate capacitive touch buttons using STM32F103. I read that the touch sense library is not available for F103. Is this c...

STM32F7 HAL DMA cache coherence and DTCM RAM differentiation

Posted on October 20, 2015 at 18:18Hello Community! I would like to know how, where, and on what conditions the DMA safety is ensured in STM32F7 HAL drivers and how DTCM is considered in them. I've generated a Cube-Project with freeRTOS for SystemsW...

i23 by Associate II
  • 2409 Views
  • 4 replies
  • 0 kudos

ST Link Utility cannot detect target

Posted on May 04, 2018 at 17:04Hi everybody,I'm currently struggling with flashing a binary file to a custom board including Murata LoRa module (type ABZ) which includes a STM32L0.Indeed, I have a ST Link, I connect it to the board using SWD with th...

bug report for stm32cubemx 4.25.0

Posted on March 20, 2018 at 08:47when use the stm32f103xx MCU  RTC module with HAL lib, the rtc init code generated with ll lib function.the steps to replay the issue.1) select MCU as stm32f103rct6;2)check 'Generate peripheral initialization as a pa...

Bruno Hu by Associate II
  • 2612 Views
  • 4 replies
  • 0 kudos