2018-01-30 5:48 PM
Hello, I have a separate MCU acting as the SPI Master, sending data in multiples of 64 bytes (anywhere from 1x 64 byte group, to 10x 64 byte groups) - all during a single transaction. So NSS goes low, 64 bytes to 640 bytes transfer (small delay between the groups of 64 bytes), NSS goes high. This is running at 4MHz and I verified this piece is working correctly via Oscilloscope. This data is coming over twice per second. The slave also has data to exchange back to the MCU, but I have not got that far yet so its all zeros for now.
For the SPI slave, I am using a STM32F103 that I configured using STM32CubeMX - clock running at 64MHz. These are the settings I made for the SPI slave in CubeMX:
This is what my main loop looks like:
while(true)
{ if(spiReady) { spiReady = false; InitSPISlave(&hspi1); } }Here is the 'InitSPISlave':
const short MAX_DEVICES_TRACKED = 10;
uint8_t txData[MAX_DEVICES_TRACKED * 64];uint8_t rxData[MAX_DEVICES_TRACKED * 64];void InitSPISlave( SPI_HandleTypeDef *spiHandler )
{ HAL_SPI_TransmitReceive_DMA(spiHandler, txData, rxData, sizeof(txData));}And here is the interrupt callback handler (I am only displaying the first two 64 byte chunks for now):
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{ SPISlaveTransferComplete(); spiReady = true;}void SPISlaveTransferComplete( void )
{ printf('SP1 Data Received: '); for(int i = 0; i < 64; i++) { printf('%lx ', (long)rxData[i]); } printf('\n'); printf('SP1 Data Received: '); for(int i = 64; i < 128; i++) { printf('%lx ', (long)rxData[i]); } printf('\n \n'); memset(rxData, 0, sizeof(rxData));}I am experiencing 2 main problems:
MAX_DEVICES_TRACKED' to 2 for instance, I get all of the SPI transfers and dump them to the screen (with the occasional first 64 bytes missing). If I start increasing the 'MAX_DEVICES_TRACKED' to 5, 10, 20, etc.It creates huge delays and I miss most of the other SPI transfers coming from the Master. At 20, it takes several seconds to re-initialize the SPI and begin a transfer. I timed all of the functions using HAL_GetTicks and nothing is taking that long.... so I don't know why this is happening?
I am using the SWO pin, J-link, and 'SEGGER J-Link SWO Viewer' to display the 'printf's.
Something else I have tried... I reset the clock settings back to stock, running everything at 8MHz, and I get the exact same delays here. This was my reasoning to up the clock speed to 64MHz (which I verified via oscilloscope by setting PA8 to MCC and I could see the clock cycle.) but this had no effect on the delay I am experiencing.
Thanks for taking a look and any help/advice is greatly appreciated!