STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PCROP Confusion

Posted on May 09, 2018 at 00:54I understand that there have been many threads about PCROP here. I am trying to understand the logic behind having to build code using mpure-code on gcc or the equivalent on other compilers that allows the avoidance of...

kirem by Associate II
  • 739 Views
  • 0 replies
  • 0 kudos

MPU regions and DMA

Posted on May 08, 2018 at 23:43I am confused over the inability to successfully setup an MPU region for the area that the DMA is using.  I am trying to get around having to use Clean and Invalidate Cache like so to guaranty the data is passed correc...

How use to nandflash on usbdevice?

Posted on May 08, 2018 at 21:03I use STM32F429IG, MT29F4G08ABADAWP that have been tested nandflash alright.I want nandflash as usb device on WINDOWS10.So, I setting USB_DEVICE and mass Storage Class and use example 'STM32_USB-FS-Device_Lib_V4.1.0'.F...

Kwon YM by Associate
  • 818 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F217 Revision 2 Bootloader

Posted on May 08, 2018 at 20:36Hi,I have a STM3221G-EVAL board with the STM32F217IGH6 and am trying to program over CAN. I checked the revision code on the chip to see what version bootloader it has and found it was a revision '2' chip. I can't find...

Problem with switching-off AHB bus to reduce power consumption

Posted on May 08, 2018 at 21:30Hi,I have a question... We use STM32F303 MCU and have configured a programmable voltage detector (PVD) to 2.9 V. At power-off interrupt is triggered and we have time till 2 V to store some diagnostic data into flash (f...

matic by Associate III
  • 736 Views
  • 0 replies
  • 0 kudos

DMA from internal SRAM to FMC missing first byte

Posted on April 30, 2018 at 03:07 I'm using a Nucleo -F722ZE to interface with an FPGA. The instruction and data cache are disabled. I have timer interrupts to set off the DMA at specific times with 128 bytes per transfer. No matter how I set up th...

Resolved! stm32f407 i2s interface sync in slave mode

Posted on July 17, 2015 at 10:58Hello, I'd like to know if there is a 'magical' way to syncronize the bit stream with the channel signal in the i2s receivers. I don't have control on the external stream ( slave mode), so the serial clock is free run...

albert2 by Associate II
  • 5985 Views
  • 12 replies
  • 1 kudos

Stop mode and clock configuration at wake up

Posted on December 28, 2017 at 07:42Hello,I'm facing an issue i cannot figure out. I'm currently working on a stm32l073 and using the following RTOS : RIOT-OS. When i wake up from stop mode, UART seems to be desynchronized because wrong characters a...

BKP0R clear after a Tamper event

Posted on May 08, 2018 at 17:13Hi,i'm working with stm32f415RG and i have a strange behaviuor with RTC.I configured RTC with LSEAlarm A Internal AlarmAlarm B Internal AlarmWakeUp : internal wakeupTamper1 Routed to AF1TimeStamp on Tamper detection ev...

Marco1 by Associate II
  • 1688 Views
  • 1 replies
  • 0 kudos