STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Connecting two image sensors to an STM32F69

Posted on May 24, 2018 at 11:13We're working on a project in which we've connected an image sensor to the STM32 DCMI.I'm now planning the next project, in which I want to connect two sensors, where only one should be active an any given moment, but ...

Unlock readout protection

Posted on August 28, 2017 at 11:43Hi Everybody,I have problem unlock readout protection with HAL library on STM32F030F4.My application need to apply lock / unlock by programming. The lock code works fine. After running lock code, RDPLevel shown in S...

CW Fu by Associate
  • 1381 Views
  • 1 replies
  • 0 kudos

Why mcu not reset on ESD test ?

Posted on May 16, 2018 at 08:54 When I run system clock through HSE(8MHz/24MHz/25MHz) and PLLCLK (multiplier PLLN and divider PLLM & PLLR) than mcu not reset by ESD.But when I run system clock directly through HSE(8MHz/24MHz/25MHz) than mcu get res...

STM32F75xxx and STM32F74xxx Reference Manual Error ?

Posted on May 22, 2018 at 21:33In RM0385, Rev 7At the top of page 957, it states 'For I2C I/Os supporting 20 mA output current drive for Fast-mode Plus operation, the driving capability is enabled through control bits in the system configuration con...

STM32L053R8 PWM for 100MHz

Posted on May 22, 2018 at 08:38Hi,I am using STM32L053R8 controller.I want to generate 100MHz, with 50% duty cycle.Can you please share the code?#stm32l053r8 #stm32l053r8-nucleo

stm32f769 dsi application problems

Posted on May 23, 2018 at 04:41Dear:   I am working on STM32F769 development board with the dsi unit.   I set the dsi clk to non-continuous mode and set dsi to LP command mode.  Then I  inited  the dsi module and started the DSI calling the the func...

CAN Bus interrupt stopped working

Posted on May 24, 2018 at 03:42 Hello everyone, I am using STM32F072C8 with MAX3051 CAN BUS transceiver to gather CAN bus data from a vehicle. Below is the main part ofmycode. while (1) { main_counter++; sprintf(print_buf1, '\r\n%d | main_c...