STM32F723e-disco HS USB examples - Cube issues
I am currently trying to generate a new project for Keil as a HS Custom HID device (eventually it will be composite with another class) and have been encountering enumeration issues. The code builds, loads, and runs, but my USB bus analyzer shows a steady streams of chirps, resets, and suspends instead of enumeration. If I modify the project with the CubeMX tool to use FS instead, the project does appear to enumerate properly so is there something else simple I may be missing here? Are there any standalone HS USB reference examples for the STM32F723e-disco, because I haven't found any yet in the F7 Cube library?
#stm32f7-usb-device-hs