STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use X-CUBE-AVS 1.0.1 for 32F746GDISCOVERY (STM32F746NG MCU), which is has hex file for 32F769IDISCOVERY ?

Posted on May 09, 2018 at 13:45I have 32F746GDISCOVERY (STM32F746NG MCU) board and wanted to use Amazon voice service on it. But the X-CUBE-AVS  1.0.1  program present on STM website is for 32F769IDISCOVERY board. Also it contains the binaries and h...

Reasons for TIM CCx ISR not firing on STM32L433

Posted on May 25, 2018 at 15:57Hi there,I have a rather odd problem and am trying to find a solution or reason for it:I am using 3 different timers on STM32L433 with 4 capture compare registers each to generate a total of 12 completely independant s...

Resolved! lwIP + STM32CubeMX

Posted on May 25, 2018 at 10:32Dear friends,I am trying to config lwIP Netconn APIs to connect my board to the TCP/IP network using STM32F107RCt6 MCU and a DP83848CVV PHY.  The only options that I change in configuration tab in CubeMX is to disable ...

Mujtaba by Senior
  • 2852 Views
  • 6 replies
  • 0 kudos

Help with Running an ILI9341 LCD Screen off NUCLEO-L476RG.

Posted on May 27, 2018 at 09:57Hi there, I'm trying to get an LCD screen driven off an ILI9341 chip to working using SPI to interface between a Nucleo-L476RG and the screen. I have tried adafruit's library https://github.com/adafruit/Adafruit_ILI934...

Max Coop by Associate
  • 1028 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L071 ADC + DMA + Multichannels Problems

Posted on May 25, 2018 at 16:51Hi all,I am working with a custum made PCB which has a STM32L071 micro and I am facing some troubles to read multiple adc inputs via DMA (because HAL IT dondoesn't work because ADC interrupts faster than ISR can excecu...

Resolved! Nucleo 32 - Unable to reach high baud rates

Posted on May 27, 2018 at 03:21 Hello, i am using a Nucleo 32 board with STM32L432KC chipset. I need to transfer data from a mems microphone over USB to the pc continuously. To do this i need a baud rate with at least 1.5Mbaud. The MCU is supp...

STM32F411 VCP USB OTG Problem (don't start)

Posted on May 25, 2018 at 02:23Hi,I am using the STM32_USB-Host-Device_Lib_V2.2.0 and more specifically the STM32_USB_OTG_Driver and STM32_USB_Device_Library.I have made running the VCP connection with an STMF405 with no problem.Now using an STMF411...