STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Part selection based on MPU presence

Posted on May 25, 2018 at 10:20Is there any parametric selection tool where I can filter in parts that implement an MPU?I didn't find this option on Cube MCU selector or on the webpage filtering tool.#stm32 #mpu

George.P by Associate III
  • 3850 Views
  • 8 replies
  • 0 kudos

Using HDMI CEC with the NUCLEO-F401RE

Posted on May 25, 2018 at 16:17Hey,I want to use my NUCLEO-F401RE to control a HDMI device with the CEC bus, is there any library out there for the F4? I found only some for the F0 or F1 out there.Thank you in advance for the help and informations.K...

CubeMX 4.24 and 4.25 issues

Posted on February 19, 2018 at 10:22Dear Team,I've migrated my CubeMX project for a STM32F412 MCU today and there are some changes which I would classify as bug.1) I've configured TIM6 as System-Timer (Timebase-Source) in the SYS-category. Since V4....

hexapod robot with STM32F4 and Camera detect of objects

Posted on May 24, 2018 at 23:43good morning  people i'm newbie in this plataform and I need a little bit of your help, I'm doing a project of a hexapod robot but I want it to detect objects with a camera module and if it loses the object that looks ...

EEPROM Emulation for the STM32 CubeF1

Posted on January 17, 2018 at 17:37Hi,In the STM32Cube_FW_F1_V1.6.0 software package i found the EEPROM example. STM32Cube_FW_F1_V1.6.0\Projects\STM32F103RB-Nucleo\Applications\EEPROMCan someone tell me how the flash reservation is handle here? How ...

MSP430 information memory equivalent inside the STM32?

Posted on May 25, 2018 at 11:17Hello,Is there inside the STM32L476 a flash memory reserved to user parameters?This memory would be the equivalent of the information memory of the msp430 competitor.If no, can I use any sector of the code memory?Can I...

Mich1 by Associate III
  • 1907 Views
  • 3 replies
  • 0 kudos

STM32F032 CAN bus

Posted on May 18, 2018 at 12:01Turvey.Clive.002‌ Barkin.Tyler.001‌Hi Clive , I'm using the STM32F072 discovery board. In that i'm using the CAN peripherals CAN_Tx and CAN_Rx .Below is the circuit diagram of my connection. I'm using MCP2551 trans...

0690X0000060BHlQAM.png

Interfacing a Bluetooth Module with STM32L0xx

Posted on May 25, 2018 at 05:35Hello STM32 community,I'm working on a project to interface a Bluetooth module(Adafruit Bluefruit LE Friend) with STM32L073RZ. I'll be using HAL drivers and STM32CubeMX in this project. I'm new to STM32 environment. I ...

Ash G by Associate II
  • 929 Views
  • 0 replies
  • 0 kudos