STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 usb_mic clock config

Posted on June 15, 2018 at 11:45hello,I'm trying to implement a USB microphone using STM32L4 discovery board.I have started with the USB device example and now trying to add the microphone.The library have given us the stm32l476g_discovery_audio.cwi...

SPI1_TRANSIT problem

Posted on June 15, 2018 at 10:33Hello, I realized a few weeks ago a code that works on a nucleo card with the following RF module X-NUCLEO-IDS01A4, this one contains SPSGRF-915. I have now adapted this program for a prototype containing the SPSGRF-8...

0690X0000060LHjQAM.png

stm32f746 disco USB CDC

Posted on June 12, 2018 at 10:07Hello,I try run a USB CDC on my eval board using USB FS. I generate from cubeMX a code with CDC, set a clocks (HCLK sets on 216MHz and 120MHz but USB clk on 48MHz) A clear code from cubeMx should cause that windows fi...

gd_jagi by Associate
  • 1351 Views
  • 4 replies
  • 0 kudos

TrueStudio update error

Posted on June 15, 2018 at 04:35Hi All, Would you please take a look at following error of TrueStudio being happened during 'Check update' ?================Cannot complete the install because of a conflicting dependency. Software being installed: C/...

关于EVCR与EVENTOUT

Posted on June 15, 2018 at 04:31我在使用STM32F103,我在资料上看到�?�以�?置AFIO_EVCR,选择�?个IO作为检测到端�?�上的事件�?�的脉冲输出。�?�设,我现在�?置了AFIO->EVCR寄存器,选择了PB0作为EVENTOUT输出�?�;根�?�GPIO�?�的外部中断/事件框图我选择PA1作为外部事件检测�?�,我�?�时�?置了EXTI_EMR,EXTI_FTSR寄存器,使得PA1是带上拉的输入�?�,开�?�事件请求,下�?沿触�?...

0690X0000060LH0QAM.png 0690X0000060LHFQA2.png