STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC calibration on STM32F207

Posted on June 13, 2018 at 03:26Hi all,I am searching for STM32F207 ADC calibration and not very clear about if the MCUs of this series do ADCself-calibration.I have also checked the data sheet and reference manual but could not find a description o...

Recovering information after software reset

Posted on June 14, 2018 at 16:39My program executes a software reset under certain conditions using  'NVIC_SystemReset();'Before executing the reset I need to set a variable that will still be accessible after the reset so the program can understand...

Resolved! Reset timer counter on Input Capture

Posted on June 14, 2018 at 01:13I have configured an timer IC channel and it is working ok however the timer counter isn't reset when I read the captured value: void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){if (htim == &htim2)    {       ...

ee06091 by Associate III
  • 5349 Views
  • 5 replies
  • 1 kudos

reset on nucleo -f401RE with even very simple main loop

Posted on May 24, 2018 at 22:20Dear Sir/Madam:I am using nucleo -f401RE with STM32 . I found the program keeps reset even with almost empty main loopthere is no way to do seftreset from the codes. only settings for hardware are system clock and some...

Resolved! Broken Forum Login

Posted on May 18, 2016 at 20:54The forum has been a mess the last few days. Only ''sign-on to forum'' seems to work, entering username/password on message replies just results in all sorts of error screens/pages. TCP connect or somesuch. #worst-f...

How to display a large JPG image?

Posted on June 14, 2018 at 20:50HiI have a STM32F746 Discovery board.  I want to show jpg images on its display as background.There is an example for small images that works, but I don't understand the part where something is actually shown. Buffers...

LMI2 by Lead
  • 771 Views
  • 0 replies
  • 0 kudos

STM32L072CZ Discovery Board PIN Layout

Posted on June 14, 2018 at 17:32Hi,I use the STM32L072CZ Discovery Board and I don�t find the PA6 PIN (MISO) on the board. In which document I can find the shematic Information? Or can somebody tell me another way to find the right PIN on the board,...

Resolved! Over the Air Update BLE, STM32F2, CRC Always 0?

Posted on June 05, 2018 at 17:21I would suggest opening the file attached in notepad++.Generally speaking the code makes sense. I can get it working without the CRC, which apparently is supposed to equal 0.Note the following section:if(psFirmware->u...

ADC & DMA disrupting SPI

Posted on June 13, 2018 at 21:48Hi,I have ADC & DMA working well, scanning 2 channels in circular mode using full and half full callback routines. It works swimmingly. I also have SPI transmissions happening off of a timer interrupt. The problem is ...