STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB VCP CDC pin connections

Posted on July 05, 2018 at 08:00Hi, I am trying to interface my SSTM32F446RE with the computer using USB VCP CDC interface. I have configured it using cubeMX and it is set up perfectly. Do i have to connect anything to USB_OTG_FS_DM USB_OTG_FS_DP Pi...

B-L072-ZLRWAN1 not working while on battery

Posted on June 03, 2018 at 18:46Dear STM32 Community, I have a B-L072-ZLRWAN1 that I have programmed using arduino and the libraries from https://github.com/GrumpyOldPizza/ArduinoCore-stm32l0. I use the board to connect to The Things Network and it ...

Bootload via UART STM32F769

Posted on July 05, 2018 at 12:48Hi,I made a LED-Blinking software for the STM32F769. I can flash the software into the MCU using JTAG and ST-LINK Utility.But I can’t update the MCU via UART. I have some issue!I tried 2 different settings:Case 1:BO...

An Ha by Associate II
  • 1084 Views
  • 0 replies
  • 0 kudos

CAN transmit error

Posted on July 05, 2018 at 12:36 Hello I have a bus with 1 master and 3 slaves, which communicates perfectly without problems. At the moment we activate the power part of the system, noise starts to be generated and suddenly one of them st...

Help with USB CDC

Posted on July 05, 2018 at 11:12I have interfaced an STM32F446RE in USB-CDC mode. I have made it device only, I set the middleware to CDC, and I set the clock appropriately too. I also added the change to CDC_Transmit_FS function. When I try to use ...

USB CDC

Posted on July 05, 2018 at 10:24Can the USB port be used for communication and power supply at the same time. What is the baud rate at which the communication happens?

STM32Cube makefile project debugging in Atollic

Posted on June 29, 2018 at 18:38I have generated a makefile project with cubemx. Furthermore, I was able to import that project in to Atollic (New->Makefile Project with Exisiting Code).I am able to successfully compile the project, however I am una...

Rav K by Associate II
  • 1767 Views
  • 3 replies
  • 0 kudos

Resolved! Freezing the IWGD Watchdog under Debug is not working

Posted on March 21, 2018 at 09:01Hello,i have a STM32F051 and use the independent watchdog.I would like the IWDG counter to stop if the core is halted.I set the DBG_IWDG_STOP in the DBG Modul, but when i stop the core with the debuger my mcu still g...