STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 ITCM testing for improved performance

Posted on July 05, 2018 at 00:44Hi all,EDIT:Intention,I would like to test if there is any performance gain to be had by running functions tat are called inside interrupts from ITCMRAM rather than flash on an STM32H7 MCU.I'm working with an STM32H7 ...

FreeRTOS V10

Posted on May 05, 2018 at 21:00The current FreeRTOS in the Cube Repo is V8.x.x.  Way down level.  Is there a reason why the repo has not been updated to V10?

tim3 interrupt not getting cleared

Posted on July 06, 2018 at 00:09I'm new to ST but have extensive experience with Eclipse and other ARM M cores..I created a simple 'blinky' program using STM32CubxMX and ST32M System Workbench on a STM32F769-DISC0 Discovery Board.The LED toggles onc...

STM32F4 timer 13 as master for timer 12

Posted on January 21, 2016 at 15:38 Can`t get the TIM12 to work in slave mode from TIM13 as master. /* TIM13 clock is 1us */ TIM13->CNT = 0; TIM13->PSC = ( TimerBusClock / 1000000U ) - 1U; TIM13->ARR = 0xFFFFU; TIM13->CCR1 = 0xFFFFU; ...

vlpasha by Associate II
  • 1603 Views
  • 6 replies
  • 0 kudos

HAL_Delay and UART problem.

Posted on July 06, 2018 at 14:09I have a problem with stm32f103, if insert in HAL_Delay(1000) in Serial Monitor i see incorrect results, but if i insert HAL_Delay(150) the results are correct. I do not understand why!This is the code:while (1) { HAL...

Power Management for STM32L4R9VI MCU

Posted on July 06, 2018 at 17:47We are currently working on a device for healthcare implementation and had chosen the STM32L4R9VI to meet our specific needs. However, we are stuck on finding a suitable battery-charge-management solution that is also...

STM32F103, HAL and timer(s)

Posted on July 06, 2018 at 12:24I created a new project (using CubeMx & Atollic TrueStudio) for STM32F103RB and tried to toggle a bit as quick as possible; I use TIMER2 and this function to initialize it:=======================/* TIM2 init function ...

RaduG by Associate II
  • 3386 Views
  • 7 replies
  • 0 kudos

OpenOCD support for STM32F469

Posted on July 06, 2018 at 16:24Has anyone ever tried to program STM32F469 discovery board using OpenOCD? I am receiving the following error. Any ideas to debug this or any leads on this is appreciated.embedded:startup.tcl:21: Error: Command/target:...