STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

extern "C"

Hello everyone, maybe it's a stupid question but in the interrupt handling function I can't rewrite a variable. I'm sure that the interrupt is triggered and assigns a value to rx_counter, read_msg is executed in a loop, but when the value of a variab...

Amrello by Associate
  • 1872 Views
  • 2 replies
  • 0 kudos

CAN_Networking code sample

I found CAN_Networking code sample in STM32Cube repository: STM32Cube\Repository\STM32Cube_FW_F4_V1.21.0\Projects\STM324x9I_EVAL\Examples\CAN\CAN_Networking. It doesn't run directly on my STM32469I-EVAL board. I have two questions:What is STM324x9I_E...

DFU mode -- Can it be entered with power on?

When I put 3.3V to boot0 and 0V to boot1 and then 0V to NRST,I don't get DFU mode. I have to cycle power withboot0 HI to the MCU to get DFU mode.The docs suggest different. have I misinterpreted the docs?Thanks, John

Jump application bootloader 0x8003000 interrupt not working

hi guys!Can you help me solve that problem:I had write bootloader for stm32F300rct6, program have jump to main application success but interrupt not working. I don't know what is missing? In main application i edit #define FLASH_BASE ((uint32_t)0x080...

TPham.10 by Associate II
  • 2630 Views
  • 4 replies
  • 0 kudos

stm32 c2c portal does not send activation emails

I registered on stm32-c2c.com website but it continue to tell me that it needs to confirm my email. I never got email with confirmation link. When I click "RESEND" button it says "Email successfully sent" but I never got any. It does not allow me to ...

ESava by Associate
  • 836 Views
  • 0 replies
  • 1 kudos

Nucleo-H743 out of stock

Posted on March 15, 2018 at 12:37I wanted to try Nucleo-H743 board to see, if H7 MCU is a good choice for my application. But it seems like there's no vendor that provides the board. I think it has been a while since the board is out of stock. Does ...

M. Jeong by Associate II
  • 3883 Views
  • 9 replies
  • 0 kudos