STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STOP mode and STM32L152~ 440 uA

Dear,I have Nucelo board with STM32L152RE. I have just made a simple project with CubeMX:After reset - blink 5 times by LED and then go to STOP mode. After pushing a button repeat whole proces again and again. Button is on EXTI13.My problem is that p...

JAN R by Associate III
  • 1099 Views
  • 2 replies
  • 0 kudos

Stack pointer for the STM32L151CB in STM32CubeMX

I am working on the readout of a GPS module on the Rak811 tracker board featuring an STM32L151CB processor. My program showed very strange effects and after longish debuggginb I found out that the stack pointer was wrongly set at entry of me man prog...

URaic by Associate II
  • 1007 Views
  • 2 replies
  • 0 kudos

CAN communication Time Out error

I am trying to send the data from stm32f103c8t6 to can analyzer but i am always getting the time out. I have uploaded my code i am using the can transceiver MCP2561. I am really struggling with this from around one month , If you can rectify my code ...

STM32-MAT / TARGET crash archive

Hello! I can not extract files from the archive en.stm32-mat_target.zip (STM32 embedded target for MATLAB and Simulink (RN0087)), which I downloaded from your site. Tell me what I'm doing wrong?

EDesh by Associate II
  • 706 Views
  • 0 replies
  • 0 kudos

ADC reading delayed to DAC output

Hello everyone,For a project I need to delay a 0->3V3 block wave with a +-400µs delay.After some searching for examples I did found a lot of examples reading an ADC input with DMA to memory. Also I did found some examples of pushing data from memory ...

Why my clock core of my stm32f is 10MHz?

Hi, I try to speed up my core because I need speed. I have routine who start PWM and I need it to be done in 1,33 microsecond. My problem here is my clock core speed is 10MHz, (according to keil uvision 5). And when I watch the assembly code, for sin...

0690X000006C0Q1QAK.jpg
RGira by Associate II
  • 1644 Views
  • 4 replies
  • 0 kudos

How to give a pulse for a certain amount of time?

I'm using a L432KC nucleo for my project. If I have some normal GPIOs (no timer channels) configured as output, how can I give a pulse for a certain period of time? Is this when One Pulse Mode comes to play?

xpp07 by Senior
  • 858 Views
  • 1 replies
  • 0 kudos

CAN transmision failed

HiI design a custom board with STM32f429. I want to send and receive messages via CAN. I can receive message but I can't send any message. I used HAL library and SPL library and they have the same result. How can i resolve it?