cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L4 VDD vs VDDUSB vs VDDA

Patrice Favreau
Associate
Posted on May 01, 2018 at 00:12

I am designing with a STM32L4 in QNF48 and would like to save power...

How about

    VDDUSB = 3.3V

    VDDA = 3.3V with linear regulator , VREF = VDDA

    VDD = 1.8V 

    Now the data sheets say  |∆VDDx| must be less than 50mv .

    

    Is this mean all power need to be at the same level +/- 50mv, or that all of the same name need to be within 50mv

 Thanks!!!

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
waclawek.jan
Super User
Posted on May 01, 2018 at 10:01

Now the data sheets say  |∆VDDx| must be less than 50mv .

Which datasheets? And how do they exactly describe what |∆VDDx| is?

JW

Posted on May 01, 2018 at 10:55

Every STM32 datasheet I ever saw.

So if this is true that all vdd need to be basically the same voltage

Can we use the USB while vdd is not 3.3V?

Thanks

Posted on May 01, 2018 at 19:55

Every STM32 datasheet I ever saw.

Show (you can paste pictures here).

JW

Jismal Jamal
Associate II
Posted on May 11, 2018 at 09:03

 |∆VDDx| must be less than 50mv  :- Variations between different VDDX power pins of  the same domain

So if VDDIO2 ,VDD ,VDDUSB are of separate domains so no issue as of my knowledge correct me if i am wrong.