The current Flash Loader does not support the STMH32H7XX family, can we hope to have support soon? The PID is 450 , It is relatively easy to fabricate a .STMAP but the option bits need to be somehow supported by the application
Posted on May 01, 2018 at 00:12I am designing with a STM32L4 in QNF48 and would like to save power...How about VDDUSB = 3.3V VDDA = 3.3V with linear regulator , VREF = VDDA VDD = 1.8V Now the data sheets say |∆VDDx| must be less than...
Posted on May 01, 2018 at 10:55Every STM32 datasheet I ever saw.So if this is true that all vdd need to be basically the same voltageCan we use the USB while vdd is not 3.3V?Thanks