STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Changing SPI modes with HAL

Hi,I am using a DAC which takes data in 24 bit format, 8 control bits and 16 data. I currently have two seperate large 8 bit and 16 bit arrays.I want to change between modes on the fly before each transfer using SPI_DATASIZE_8BIT / 16BIT, but it stay...

Matt G by Associate II
  • 1478 Views
  • 2 replies
  • 0 kudos

Resolved! ADC error in reading voltage

Hi everyone,I'm having troubles with the internal ADC (STM32F072CBTX): a significant offset is present in the values provided by the converter. I performed a set of test measurments on the ADC: the results are shown in Table1.jpg.Where:Vmis is the vo...

MCivo by Associate
  • 4285 Views
  • 2 replies
  • 0 kudos

Resolved! Board support package for STM3240G-EVAL board.

Hi,I am using Keil V5.26.2.0. Although I have installed DFP for my particular MCU, from where I may get bsp for my board. Please be gentle guys, I am pretty new to the world of MCUs.Cheers and a happy dayTahir

MRana by Associate II
  • 5221 Views
  • 10 replies
  • 1 kudos

Setting DAC1 ch1 DAC2 ch1 on STM32F303k8

ST community,The issue I’m having is getting DAC2 to work, DAC1 works great. I’m using TrueStudio no HAL, everything setup manually. I’m receiving data from PC to mic USART then adjusting Vout on DAC1 and hopefully DAC2. The main question is I can’t ...

BBuch by Associate
  • 924 Views
  • 1 replies
  • 0 kudos

How to re-Mount SD-Card after pulling out SD-Card.

I can't re-mount SD-Card after pulling out and inserting SD-Card again.It shows "FR_DISK_ERR" when error occurs.Please let me know if there is anything I have to follow.I have CubeMX ver 4.22, FreeRTOS and HAL Driver.=================================...

spark.72 by Associate
  • 836 Views
  • 0 replies
  • 0 kudos

trying to understand systick and timer at STM32L1xx

Posted on March 19, 2014 at 08:26Hello,I'm using STM32L152 discovery board.I'm trying to define systick for 100mSec, and tim2 to 1 sec.After measuring the pin togeling with scope, this is what I came up with:I know SystemCoreClock is 32MHz.For systi...

zoharr by Associate II
  • 1795 Views
  • 4 replies
  • 0 kudos

Going to DFU mode programmatically STM303RE

Hi,I hav difficulties going to DFU mode programmatically. In the en.DM00070391.pdfpage 19, saysThe embedded boot loader is located in the System memory, programmed by ST duringproductionbut does not specify the start address. I tried en.CD00167594.pd...

Marius CO by Associate III
  • 700 Views
  • 1 replies
  • 0 kudos