cancel
Showing results for 
Search instead for 
Did you mean: 

NEW TO STM32F407 DISCOVERY BOARD

Yadav
Associate II
Posted on June 03, 2018 at 09:02

Hi Everyone, I m new to STM32F407 DISCOVERY board. Before i have worked with AVR micro controllers. Now i want to develop a wireless home automation application with STM32. Can anyone help me out with the recommended IDE and examples ?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 03, 2018 at 17:11

Cube/HAL is the current library (download CubeF4 package)

STM32Cube_FW_F4_V1.21.0\Projects\STM32F4-Discovery\Applications

STM32Cube_FW_F4_V1.21.0\Projects\STM32F4-Discovery\Examples

Keil and IAR should work equally well

They is plenty of material for this board on the internet,

Joseph Yiu's Essential Cortex-M3/M4 would be a good book when migrating to the platform. The Reference Manual and Programming Manual for the F4 should also be reviewed.

The STM32F4-DISCO is quite an old platform, you might want to consider some of the new families and NUCLEO/DISCO boards providing serial connectivity, Ethernet, and Arduino shield options.

There is an L4 IoT board with multiple radios which might be a good fit for Home Automation applications.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..