STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G0 ADC channels availability and GPIO mapping

Hi There, I am currently using the STM32G050C8T6 (LQFP48) and would like to use PA11 as an ADC input, based on the datasheet: DS13514 - Rev 2 specifically table 12, it appears it can be used as ADC_IN15, However in STM32Cube IDE , PA11 can not be ass...

AndFel_0-1743370150027.png AndFel_1-1743370433676.png
AndFel by Associate II
  • 1737 Views
  • 3 replies
  • 0 kudos

Resolved! How is SCLH and SCLL calculated in I2C_TIMINGR?

I have read the document RM0433 and AN4235, but the calculation is still a puzzle. For example, if my I2C frequency = 1MHz, I2C clock source frequency = 170MHz, AF=on, DF=off, rise time = 80ns, fail time = 10ns, how do you get the SCLH = 0x10 and SCL...

SHU.1 by Associate
  • 3404 Views
  • 2 replies
  • 0 kudos

NUCLEO-H723ZG BOARD ADC NOISE

Hi, I am planning on using STM32H723ZGT6 chip on one of my boards. I got the NUCLEO-H723ZG to measure the 12-bit ADC noise. From the datasheet for STM32H723ZGT6, the max ADC noise should be 5 times the LSB or 4.02mV. (1 LSB = 3.3/4096) I am getting 2...

josegalicia_0-1741886842223.png

Resolved! DBANK Option Byte default STM32G4

What is the default value of the DBANK bit in STM32G4 MCUs. According to the reference manual, flash memory address 0x1FFF 7800 has that option bit, and the ST production value is 0xFFEF F8AA, which would make DBANK default to 1. Does this mean STM32...

tomm5771 by Associate III
  • 1266 Views
  • 2 replies
  • 1 kudos

Resolved! GP and N version ICs

Hi,I am using STM32C071CBT6 chip on my custom board. From datasheet, i could see that there are two versions available - GP and N version. Part number section of datasheet mention about 3 more characters after this part no. to identify if it is N ver...

PPate1_0-1743594616574.png PPate1_1-1743594767820.jpeg
PPate.1 by Associate III
  • 1212 Views
  • 1 replies
  • 0 kudos

Resolved! Implementing STM32L4S5ZIT6 Bootloader with a Memory Marker

Hello, I am working on the development of a bootloader for the STM32L4S5ZIT6, and I need help to implement a feature where the bootloader is triggered after receiving a user request in the main application (the main app saves a marker in memory). Her...

ZAYN by Associate II
  • 1278 Views
  • 2 replies
  • 2 kudos

Help with Ethernet on STM32 H723ZG

Hi all! I have been using a F446RE board to communicate with an encoder using SPI. I get back a 16-bit value every ms (the process runs at 1kHz). However, I now need to transfer the acquired data over ethernet (it has to be ethernet, not UART or anot...

Screen Shot 2024-06-21 at 2.07.16 PM.png Screen Shot 2024-06-21 at 2.07.44 PM.png Screen Shot 2024-06-21 at 2.08.06 PM.png Screen Shot 2024-06-21 at 2.08.19 PM.png
shuyu_vk by Associate
  • 4435 Views
  • 5 replies
  • 2 kudos