STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can't send TCP message exactly more than 1000 times

HiI'm using STM32F439 Dev Board and LWIP as TCP/IP stack; I'm using TCP echoserver example. the board is connected to PC. when I send a message from PCto the board, it echoes back the message. But there is a problem. aftersending exactly 1000 message...

HI i am trying to get the example project for interfacing USB stick into my custom board which has STM32F429II now , I could not find it in any of your latest Cubeprjects or anywhere in example projects,

I want to know how do i interface the USB stick to my board and start communicating with it.basically i want to read .bin/.png/.dfu files from USB stick Please provide the example project as soon as possible 

Vprabhu by Associate II
  • 865 Views
  • 3 replies
  • 0 kudos

Hi, I try to configure the ADC of a STM32F407 to work in triple injected simultaneous mode, but only ADC1 works. How do I have to configure the ADC's that they work simultaneous?

As stated in the Reference manual. I configure the master ADC1 to get the trigger from the TIM2 TRGO and this ADC1 is working when started. ADC2 and ADC3 start only when I configure JEXTEN (=0x01) and JEXTSEL (=0x03) in CR2 of the according ADC. I do...

ATasc by Associate
  • 714 Views
  • 0 replies
  • 0 kudos

Is it possible to get Vbus disconnect notification on self-powered USB HS device in STM32H743 without wiring VBus to an IEXT port?

I have a working USB2 (ULPI) device mode interface, and want to detect cable removal. There appears to be provision for this: OTG_GINTSTS has SRQINT and OTGINT bits and OTG_GOTGINT has the OTGINT bit, but I do not seem to get any response to cable r...