STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 signalling for RS-485 - DE?

We are using the STM32F091RC to setup an RS-485 interface with the TI SN65HVD11. How do we connect to the DE control signal for the SN65HVD11? I have currently selected USART3 -R - PC5 (RX)D - PC4 (TX)DE - PB1 (RTS) Is this correct? Also what is CK_R...

Justin1 by Senior
  • 1090 Views
  • 1 replies
  • 0 kudos

SDIO works well in SD-1bit mode but not in SD 4bit mode

I am using cubemx generated SD card test code on a custom board. And everything looks fine in SD 1bit mode, I can create new file, read and write data to it correctly. But when I am using 4bit mode, the f_open() function stalls. What might be the pro...

Yang Yang by Associate III
  • 1223 Views
  • 3 replies
  • 0 kudos

STM32H7 AXI bus clock stopped in CSleep?

According to RM0433 revision 5 section 7.5.12, “The AXI bridge clock is enabled when the CPU is in CRun mode.�? Does this mean that the AXI bridge clock is disabled (and presumably things connected to the AXI, like the MDMA) do not work in CSleep? Th...

CHead by Associate III
  • 672 Views
  • 0 replies
  • 0 kudos

Possible ways to save 40Kbytes/Second?

I would like to know what are the possible ways to save 40KBytes per second? what type of memory devices do i have to use. I presumed of using class 10 memory card but it has only 10Mbitspersecond (= 1250KBytes/second). I would have to store atleast...

Apill by Senior
  • 584 Views
  • 1 replies
  • 0 kudos

Disabling a timer after PeriodElapsedCallback is called

So I have two timers, one in OC mode and one in IC mode. The IC waits until the OC toggles, it registers the value and waits for it toggle again to record a second value. What I want to do is after the OC timer has toggled twice is for it to disable ...

FFuma by Associate II
  • 1144 Views
  • 1 replies
  • 1 kudos

Resolved! HSI/2 before PLLSRC in STM32F030xC ?

Posted on January 26, 2018 at 18:50Hi,I have a problem with the PLLSRC of a STM32F030RC : to obtain 24MHz for the sysclk I have to use PLLMUL @ x6 with HSI (8MHz) but 6x8 = 48MHz ?If I output the sysclk on a MCO pin (with no div) I have actually 24M...

Peter M by Associate II
  • 4279 Views
  • 12 replies
  • 0 kudos