cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F479IIT6

Posted on July 04, 2018 at 12:19

we are using STM32F479IIT6 in our design as below,

1.USB 2.0 full speed

2.Self powered

3.As device

Could you clarify on the following points,

1.what is default configuration of OTG_FS_ID(left unconnected,GND or pullup)

2.since it is self powered,there is no need of 5V supply(VBUS is used for sensing of host connection)

Thanks,

Arun D.

#stm32f479iit6-usb-id
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Khouloud GARSI
ST Employee
Posted on July 05, 2018 at 16:05

Hi

arunkumar.devershett

,

Khouloud.

Posted on July 05, 2018 at 16:20

Hi Khouloud,

I have referred the attached application note however it is not mentioned about OTG_FS_ID, also given snapshot below.

As ID pin is required in OTG applications only, can with go with unconnected.

Kindly help us in getting configuration of OTG_FS_ID in USB 2.0 full speed as a device/peripheral.

Thanks,

Arun D.

________________

Attachments :

image001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxRQ&d=%2Fa%2F0X0000000ay6%2FrVu9PICuS90fAcYxP5gY4TjPP9oU3BNkzzzUMEj8iwk&asPdf=false

Application note_USB hardware using STM32 MCU.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxRL&d=%2Fa%2F0X0000000ay5%2FWx7v_OKNehFRTOuSorN2g.JZ8P8sTsyOuwosQnaArAU&asPdf=false