STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK_CLI.exe Family device :Unknown device

Hello there,I am trying to connect to a stm32F091 mcu through st-link_cli. The problem appears when the CLI cannot recognice the device, but when I use the STM32 ST-Link Utility (the one with GUI) there are no problem in find the device. Anyone coul...

MP??r by Associate
  • 1336 Views
  • 1 replies
  • 0 kudos

Any sample projects Using stm32 F407g-disc1 board

Guys this is very popular board. Is there any good source where projects are made using this board(I mean using the peripheral available on this board) are available? So simple applications, Using C or C++? Any IDE.

MRana by Associate II
  • 1534 Views
  • 2 replies
  • 0 kudos

4-wire JTAG interface not working on STM32F7.

Hi all, I just got new hardware. As we needed one more pin on our processor, and we always left the JTAG-Reset Pin floating on our last designs, I switched from 5-wire JTAG to 4-wire, which leaves the JTAG-Rest Pin free. Now, I set up my SW environme...

GW1 by Associate
  • 1913 Views
  • 3 replies
  • 0 kudos

Problem with stm32f745 work

After the firmwared (or power off-on) and after the reset the same program takes a different amount of time in ticks. Find it in my oun code. Then tried to create code in Cube and check it - same thing. Then I checked clocking settings and frequency ...

kitty7c6 by Associate II
  • 3791 Views
  • 10 replies
  • 0 kudos

Over The Air Upgrade in stm32f407

Hi everyone, I am using stm32f407zet6 MCU and i am integrating SIM7600E GSM module with microcontroller. I want make Over The Air Upgrade of my firmware. What are the steps to be followed to achieve OTA update in my microcontroller. How to achieve ...

f_write dropped 3 bytes

Hello, sorry for posting this post again. I have a problem with my code. I'm trying to write a program to take picture from camera and save it as motion jpeg video (MJPEG) in to USB. I build already the header and the structure of MJPEG file but it's...

0690X000006CXhBQAW.png

CAN Buffer designing RING FIFO engine

Hello, Ok have a problem that I would like to over come , I am developing with CAN and the Nucleo st32F446re board.All is working and I can send and and receive packets of CAN data, but..... I would like to implement a more fail safe engine to deal w...

0690X000006CZ8cQAG.jpg
JHERI by Senior
  • 2075 Views
  • 5 replies
  • 0 kudos