STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-ESC001V1 always Over current error.

After a view short tests with the ST Motor Profiler the Rotor seemed to stall.(Lab-powersupply 22V 9A)Then smoke appeared (not sure where exactly)Now every time i want so start the Profiler it says "Over current".Even when i set the maximum current t...

0690X000006CKjCQAW.png 0690X000006CKjHQAW.jpg
TR?�g by Associate
  • 1739 Views
  • 3 replies
  • 1 kudos

Unique ID and STM32F030

Hello,STM32Cube_FW_F0_V1.9.0 lists UID_BASE for all STM32F0 devices, including STM32F030x6. As I remember, some F0 parts don't include a unique ID for cost reasons. Either my information is false or UID_BASE should only be listed with unique ID avail...

BOOT1 in STM32L071KZ

HiI see there is no boot1 in L071So bootloader mode is with boot0 = "1" only ?I'm not missing anything ?​Thanks

ER7 by Associate II
  • 1385 Views
  • 2 replies
  • 0 kudos

BFB2 and bootloader flash-bank selection

Posted on February 23, 2016 at 18:15I've recently delved into this subject because I need to design a firmware upgrade mechanism on the STM32L4xx.  The documentation is pretty much useless, as it is not only incomplete, but contradictory too.  I'm g...

mhaun by Associate II
  • 10448 Views
  • 14 replies
  • 1 kudos

STM32L475RC RTC Issue?

Are there any known issues with the RTC Wakeup on the STM32L475?I cannot get it to work, I've copied the code exactly as it appears in the STOP2_PWR example, but no matter what I do the ISR does not get called.If I check the registers I can see the t...

adrian by Associate III
  • 2035 Views
  • 3 replies
  • 0 kudos

Is SafeRTOS support in STM32CUBEMX?

If I want to use the SafeRTOS for critical issue can I use it in the cubeMX as I use today the FreeRTOS?If it is possible or not at this stage, and if yes what adaptation do I need to do to use it?Is there any guide for immigrate Safe RTOS to CUBEMX?...

Barbie by Associate II
  • 1254 Views
  • 1 replies
  • 0 kudos

STM32G0 Series Information

I noticed a new STM32G0 series (Cortex-M0+ core) support in the latest STM32CubeMX. Is there any information available to general public about this new series? Thanks.