STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLink and target Supply Power

I am working with a STM32L0538 discovery board and am ready to move to my own target board. According to the documentation I can use the STLink/V2-1 portion of the discovery board as the debugging interface for my target board using the CN5 connector...

erussell by Associate II
  • 1092 Views
  • 1 replies
  • 0 kudos

JTAG to SWD problem with STlink

Hi,I use ST-Link/V2 programmer. I connect my stm32f407 with this circuit to my programmer.Everything works OK.I tend to connect my JTAG connector to SWD pins in my board But when I disconnect Reset or VCC pins from my programmer ( while my board is p...

0690X000006CkDYQA0.png 0690X000006CkDiQAK.jpg
parisa by Senior
  • 893 Views
  • 1 replies
  • 0 kudos

Speed limit in the DCMI and the FMC in STM32H7

The DCMI controller in STM32H7 is faster than F4 and F7. It supports a pixel clock up to 80Mhz. However, is the FMC controller fast enough to acquire such fast data? Let's say, one has an image sensor that generates 10-bits or 12-bits data with 74.25...

M. Jeong by Associate II
  • 2347 Views
  • 3 replies
  • 0 kudos

Problem: Not generating files

Posted on January 28, 2016 at 20:57The STM32Cube does not generate some .c and .h files for my code.I'm using MDK-ARM V5 toolchain for my project.Whenever I try to create another project the missing files change in random fashion, sometimes its mxco...

joao23 by Associate II
  • 6385 Views
  • 12 replies
  • 0 kudos

recommendation on OS/IDE

Hi all - I'm beginning a project that will utilize the STM32L496ZGT6. It's been several years since I've worked in the STM world, so my knowledge of available software is quite dated. I'd like to hear any feedback on the following:I want to use an OS...

mzimmers by Associate II
  • 1892 Views
  • 3 replies
  • 0 kudos

Why my STM32 doesn't start to run ?

After upload my program into a stm32F103C8T6, the program doesn't start. I just use STM32CUBE-MX to configure my mcu, and I just add some blinking on 5 output (push/pull). But after reset my output seems to stay in high inpedance ? Does Mcu start its...

fDNTI by Associate II
  • 2986 Views
  • 7 replies
  • 0 kudos