Is there available older version of X-CUBE-SUBG1 package? Where can i download it?Last version (en.x-cube-subg1_firmware3.1.0 and en.x-cube-subg1_firmware3.0.0) have some problems. I want to read data from WM-Bus meter using T2 mode in "OTHER" mode.I...
Hello.Can i read state of BOOT0 pin in STM32F030F4P6?My uC always turn on with BOOT0 GND, but i need to have dual purpose pin BOOT0 and have possibility to read only state of this pin.
I just think that if i can set BOOT1 by software that is also possible to read BOOT0 throught some registers.I check SYSCFG and it stays all 0 even if i pull up BOOT0 pin.It looks that i have to short pin 1 (boot0) and 2 and then read state.